We use cookies to give you the best experience on our website. If you continue without changing your cookie settings, we assume that you consent to our use of cookies on this device. You can change your cookie settings at any time but if you do, you may lose some functionality on our website. More information can be found in our Privacy Policy.
These tutorials explain the principles of steam engineering and heat transfer. They also provide a comprehensive engineering best practice guide covering all aspects of steam and condensate systems; from the boiler house and steam distribution system up to the point of use; through the condensate recovery system and returning to the boiler. Virtually all major applications and products are discussed.
The introduction of steam as a useful and powerful purveyor of energy. It discusses the versatile uses and benefits of this ubiquitous vapour; and the ways in which it is produced and distributed to achieve maximum performance and economy for the end user.
This introductory tutorial describes the many benefits and uses of steam in industry today.
The benefits of steam are viewed differently by individuals according to their role and priorities. This tutorial explains the issues of most importance to chief executives, managers and operators and how steam can address these issues.
How is steam generated, distributed, controlled and used? How is the condensate recycled? A basic overview of a steam system.
Properties of various types of steam are considered, along with basic heat transfer principles and how to calculate consumption rates for process applications. Entropy is tackled in simple terms, removing unnecessary fears often associated with the subject.
An overview of the units of measurement used in the Steam and Condensate Loop including temperature, pressure, density, volume, heat, work and energy.
The properties of steam explained here, including the ability of steam under pressure to carry, and then give up, large amounts of energy. Topics include saturated steam tables, dryness fraction and flash steam.
An explanation of the properties and uses of superheated steam (such as for electricity generation). Including explanations of the Rankine and Carnot thermodynamic cycles, superheated steam tables and the Mollier (H-S) chart.
Steam should be available at the point of use in the correct quantity, at the correct pressure, clean, dry and free from air and other incondensable gases. This tutorial explains why this is necessary, and how steam quality is assured.
Steam is often generated to provide heat transfer to a process. Modes of heat transfer (conduction, convection, radiation) within or between media are explained, together with calculations and other issues such as heat transfer barriers.
How to calculate steam requirements for flow and non-flow applications. Including warm-up, heat losses and running loads.
Methods of measuring steam consumption, from the very basic to sophisticated flow metering, are explained in this tutorial.
Design ratings for items of plant can be both helpful and misleading, as changing any factor can alter the predicted heat output. Also, how to calculate steam load requirements from the kW rating.
The heating of liquids in tanks and vats is an important requirement in process industries. There are many types of tank with different uses. Determination of heat requirements, heat transfer and heat loss calculations are all covered in this tutorial.
Indirect heating of fluids is covered in this tutorial including layouts, control and drainage of coils and jackets, and heat transfer calculations.
Direct steam injection involves the discharge of steam bubbles into a liquid at a lower temperature to transfer heat. This tutorial explains the process and the methods used, including the relevant heat transfer calculations.
Steam will condense and give up its enthalpy of evaporation on the walls of any pipe or tube at a lower temperature. It is not usually possible or necessary to calculate steam consumption exactly. This tutorial allows satisfactory estimates to be made for most practical purposes.
Different types of heat exchanger are explained and compared in this tutorial, together with steam consumption calculations and other issues such as the relevance of the starting load.
The steam consumption of other common plant items, including heater batteries, calorifiers, drying cylinders, presses and tracer lines.
Entropy is a concept some find difficult to grasp, but in truth it does not deserve such notoriety. Look upon Entropy as a road map that connects thermodynamic situations. This tutorial hopes to shed some light on this subject, by approaching it from first principles.
Entropy can be used to understand thermodynamic applications from first principles. This tutorial gives practical examples of how this can be done.
Various types of boilers and fuels are discussed, alongside the best ways in which to get the best out of this important part of the steam plant. All associated boiler equipment is considered, including basic deaerator and accumulator theory.
An overview of boiler regulations, with an evaluation of fuel types and comparisons
Overview of the different types of shell boiler with layouts, heat and steam release considerations plus pressure and output limitations
Description of water tube boilers including operation, types and benefits; also, a brief synopsis on how they are applied to combined heat and power generation.
An explanation of specialist boiler types and other specialist features.
This tutorial explains the three most commonly used boiler ratings: The 'From and at' rating for evaporation, the kW rating for heat output, and boiler horsepower.
A broad overview of the combustion process, including burner types and controls, and heat output and losses.
An overview of the necessary fittings, accessories and controls for a boiler from nameplates and safety valves to gauge glasses and level controls.
This tutorial looks at steam header arrangements and other design considerations necessary for efficient warm-up, good steam quality and proper steam distribution from the boiler house.
A look at the chemistry of water supplies including hardness and pH values.
A steam boiler plant must operate safely, with maximum combustion and heat transfer efficiency. To help achieve this and a long, low-maintenance life, the boiler water can be chemically treated.
All aspects of the design, construction and operation of feedtanks and semi-deaerators, including calculations.
The need to measure and control the total dissolved solids (TDS) in the boiler water boiler water, and the methods used to do so, including closed loop electronic control with conductivity sensors.
Boiler water is blown down to control the amount of total dissolved solids (TDS) in the boiler. This water is pressurised, hot and dirty, creating large volumes of flash steam and possible disposal problems. A heat recovery system can reclaim large amounts of energy during this essential process.
Factors surrounding the removal of suspended solids from the boiler, including valves, piping and blowdown vessels, with calculations.
The level of water in a steam boiler must be carefully controlled, to ensure good quality steam is produced safely, efficiently and at the correct pressure.
The application of level controls and alarms, plus an overview of different level detection methods, including float-type controls, conductivity probes and capacitance devices.
A detailed explanation of on/off, modulating, two and three element automatic level control, with a comparison of pros and cons.
The function of high and low level alarms. Low-level alarms will draw attention to low boiler water level and, if required, shut down the boiler. High-level alarms protect plant and processes.
The pros and cons of direct versus externally mounted level controls.
Requirements for regular testing will vary according to national regulations, and the type of equipment installed.
The need to remove gases from boiler feedwater and the operation of a pressurised deaerator, plus calculations.
A complete overview of the need for steam storage to meet peak load demands in specific industries, including the design, construction and operation of a steam accumulator, with calculations.
Fluid characteristics and flow theory (including Bernoulli's theorem and Reynolds' numbers) are introduced and developed to provide basic metering theory and techniques. Different meter types, instrumentation and installation practice are also discussed.
Users may wish to measure the flow of steam to help with plant efficiency, energy efficiency, process control or costing purposes. This tutorial considers the characteristics of flowing fluids and the basic requirements for good steam metering practice.
A detailed examination of the principles and terminology surrounding the topic of flowmetering, including accuracy, repeatability and turndown. Also included is a basic insight to Bernoulli's Theorem.
The operation, advantages and limitations of different types of steam flowmeter, including orifice plate, variable area and vortex shedding devices.
Apparatus for accurate steam flow measurement, including differential pressure cells and data collection & analysis equipment. Also covers special considerations such as the effects of pressure variation, steam dryness fraction and superheat.
System design, installation and maintenance considerations for steam flowmeters, including the use of strainers, separators and flow straighteners, together with piping layouts. Includes a useful checklist for selecting the correct type of flowmeter for an application.
Control theory is discussed from fundamental proportional action to PID control. The dynamic of the simple control loop is discussed, alongside practical issues of choosing the best system for the application, and installation and commissioning issues.
This tutorial provides an introduction to the subject of automatic control, including the basic elements of a control system, different control functions, and relevant terminology, with some emphasis on safety, and stability & accuracy of control.
This tutorial looks at on/off and continuous control modes. It introduces proportional, integral and derivitive control actions and explains some of the terminology.
An explanation of each component of a control system, including valves, actuators, sensors and controllers; together with an introduction to methods of control and system dynamics, including simple control loops and feedback systems.
This tutorial will concentrate on available automatic control choices (such as self-acting, pneumatic or electric) and the decisions which must be made before selection. Guidance is offered on the basis of the three most important considerations of safety, stability and accuracy.
Practical installation and commissioning advice for valves, actuators, sensors, controllers and more.
A look at the more recent developments in control involving the use of information technology.
Control valve capacities and characteristics are investigated, along with theory and practical advice on how to size them for water and steam systems. Actuators, positioners, and controllers are introduced plus their overall effect on the control loop.
This tutorial briefly describes the basic components of different types of linear and rotary action control valves available for use in steam and water systems.
Valves need to be measured on their capacity to pass fluid. To enable fair comparison, valves are sized on a capacity index or flow coefficient. This tutorial explains the different types of flow coefficient in use, how they are established, how they compare, and typical values for different sized valves.
This tutorial briefly describes how to use flow coefficients to size valves for water systems, the difference between using two-port and three-port valves and the effect of these valves on pressure drop, flow and water system characteristics. Also explained is the importance of valve authority, and the cause and effects of cavitation and flashing under certain conditions.
Sizing a control valve for a steam application can be a complex matter. This Module attempts to throw light on the subject by using first principles to explain the relationship between flow and pressure drop. It uses a simple nozzle to explain the phenomenon of critical pressure, and how this can be predicted for steam flow through a control valve. It continues by discussing other properties such as noise, erosion, and how steam is dried or superheated as it passes through a valve, and gives various examples of such calculations. It also briefly compares shell & tube and plate heat exchangers, and shows how to use simple Kv charts to size steam valves.
Various types of flow characteristics are available. This tutorial discusses the three main types used in water and steam flow applications: fast opening, linear, and equal percentage flow; how they compare, and how (and why) they should be matched to the application in which they are used.
Control valves need actuators to operate. This tutorial briefly discusses the differences between electric and pneumatic actuators, the relationship between direct acting and reverse acting terminology, and how this affects a valve's controlling influence. The importance of positioners is discussed with regard to what they do and why they are required for many applications.
Controllers and sensors are important parts of the control system; without information from the sensor, the controller cannot make a decision and instruct the valve to move. This tutorial briefly discusses the different types of controllers and sensors available and how they operate. A brief explanation of digital and analogue control signals is also given.
Basic self-acting control theory is discussed, alongside the different types of direct-acting and pilot-operated valves, controllers, and applications for the proper selection of temperature and pressure control of steam and water systems.
This tutorial gives a basic introduction to what self-acting temperature control systems are and how they operate. The various different types of valves and controllers are briefly discussed along with typical applications for steam and water systems.
Four different types of temperature controllers are considered, including fail-safe high limit protection. Popular applications for self-acting controls are listed for process, heating and cooling systems.
Various types of self-acting pressure controls are examined in this tutorial, including direct acting bellows operated and diaphragm operated valves, and pilot operated valves, with guidelines on how to select and install them correctly. Pressure reducing valves are considered together with pressure maintaining valves and surplussing valves, alongside some typical applications.
A brief summary of, and advice on, temperature, pressure, flow and level control methods to suit various types of steam applications, with consideration to surplussing control, differential pressure control, and cascade control and installation thereof.
There are many good reasons for reducing (and sometimes maintaining) steam pressure. This tutorial details common applications for direct operating, pilot operated, pneumatic, electric and electropneumatic pressure control systems, including the advantages and disadvantages of each different control method.
Temperature control of the process can be affected using electric, pneumatic, electro-pneumatic and self-acting controls. This Module details some common applications including process vessels, heat exchangers and high temperature fail safe control.
A range of level control systems and methods are used in industry. Systems may be based on the use of floats, probes or even more sophisticated technology. This tutorial studies the use of probes to provide adjustable & non-adjustable on/off control, and modulating control of liquids. Simple flow control applications are also considered.
The service life and accuracy of a control system can be influenced by installation factors. This tutorial discusses the basic important considerations including the positioning of equipment and wiring, radio frequency interference, and protection from the environment.
Arguably, the most important subject in the generation, distribution and use of steam. Why are safety valves required? What different types are available and how are they selected, sized and installed? Other protection devices are also shown in some detail.
Any pressurised system requires safety devices to protect people, processes and property. This tutorial details situations when overpressure may occur, the wide and often confusing types of device on offer, how such devices operate and the many codes, standards and approval authorities to note.
A full explanation of the many different types of safety valves available, including operation, materials of construction and accessories.
Choosing and commissioning the correct safety valve, including selection considerations, setting, sealing, positioning and the effects of backpressure.
An in-depth study of the sizing process for a range of applications, including sizing equations for AD Merkblatt, DIN , TRD, ASME, API, BS6759 and others. Covers more complex issues such as two-phase flow and superheat.
Important installation advice, including handling, plant conditions, pipework configuration, markings and noise considerations.
Other methods of relieving excess pressure explained; plus a useful terminology section.
Efficient distribution gets clean dry steam to apparatus at the right pressure. Pipe sizing, essential drainage techniques, pipe support and expansion, air venting, and heat transfer calculations are included to help the system designer and practitioner.
An efficient steam distribution system is essential if steam of the right quality and pressure is to be supplied, in the right quantity, to the steam using equipment. This tutorial looks at a typical circuit.
Pipe sizing is a crucial aspect of steam system design. This tutorial offers detailed advice on standards, schedules, materials and sizing for various saturated and superheated steam duties.
Issues surrounding the structure, layout and operation of a steam distribution system, including condensate drain points and branch lines, the avoidance of waterhammer and the use of separators and strainers for steam conditioning.
Any steam system must be fully supported, able to expand during operation and sufficiently flexible to allow movement as a result. This tutorial includes advice on different methods and full calculations.
The venting of air and other incondensable gases from steam systems, and the provision of adequate insulation, are vital to ensure steam plant efficiency, safety and performance.
How steam traps work and why steam traps are necessary. All is explained in this block, along with the different types, where they are used, and how they are selected. Air venting theory and applications are touched upon, along with steam trap maintenance.
The duty of a steam trap is to discharge condensate, air and other incondensable gases from a steam system while not permitting the escape of live steam. The need for steam traps, considerations surrounding their operation, basic modes of operation and relevant standards are all covered in this tutorial.
Thermostatic traps operate in response to the surrounding steam temperature. The operation and benefits of 3 different types are considered here - liquid expansion traps, bimetallic and balanced pressure thermostatic traps. Each operates in a different way and is suited to specific types of application.
Mechanical steam traps rely on the difference in density between steam and condensate in order to operate. They can continuously pass large volumes of condensate and are suitable for a wide range of process applications. Types include ball float and inverted bucket steam traps. This tutorial considers the operation and benefits of both types.
Thermodynamic steam traps have a unique operating principle which relies on the dynamics of water and flash steam. They are simple, robust and reliable and can operate up to very high temperatures and pressures. Their construction, use and benefits are detailed here.
Application type, system design and maintenance needs will influence the performance and selection of steam traps. Factors such as waterhammer, dirt, steam locking, group trapping, vacuum conditions and temperature control of processes are discussed in this tutorial.
Selection tables and advice on trap selection for a range of different processes are included in this tutorial, including steaming ovens, bulk storage tanks and autoclaves.
Selection tables and advice on trap selection for a range of different processes are included in this tutorial, including multi-bank pipe dryers and rotating cylinders.
Selection tables and advice on trap selection for a range of different processes are included in this tutorial, including calendars, garment presses, dry cleaning machines and tyre presses.
Selection tables and advice on trap selection for a range of different processes are included in this tutorial, including boiling pans, retorts, digesters, coppers, reboilers, evaporators and vulcanisers.
Selection tables and advice on trap selection for a range of different processes are included in this tutorial
Selection tables and advice on trap selection for different types of steam mains, headers and off-takes are included in this tutorial, together with process vats and pressure reducing valve stations.
The presence of air has a devastating effect on steam systems and processes. The basic theory of air venting is explained in this tutorial, plus advice on air vent location.
Some of the many different applications for air vents are described in this tutorial, including steam mains, bypasses, jacketed vessels and rotating cylinders. Other issues such as venting large volumes of air, group air venting and the substitution of thermostatic steam traps are also considered.
Indiscriminate maintenance of steam traps wastes money. This tutorial considers a planned approach to steam trap testing and maintenance, with recommended methods and equipment.
A large amount of inaccurate and misleading information has been written on this subject. This tutorial gives clear, accurate information regarding the energy consumption of different trap types.
These are often neglected to save costs; but strainers, stop valves, check valves, separators, gauge glasses and vacuum breakers all have their part to play in an efficient steam system. This block explains why, and explores the different types available.
Isolation valves are used for diverting process media, facilitating maintenance, equipment removal and shutdown. The operation, application and construction of gate, globe, piston and diaphragm valves are studied in this tutorial.
Isolation valves are used for diverting process media, facilitating maintenance, equipment removal and shutdown. The operation, application and construction of gate, globe, piston and diaphragm valves are studied in this tutorial.
Check (non-return) valves are installed in pipelines to allow flow in one direction only; helping to protect equipment and processes. The operation, benefits, applications and selection of different designs, including lift, disc, swing and wafer check valves are explained in this tutorial.
Strainers arrest pipeline debris such as scale, rust, jointing compound and weld metal in pipelines, protecting equipment and processes. This tutorial considers the range of strainer and filter types in use and how to size and select them for different applications.
'Wet' steam is a major concern in a steam system as it can cause process and maintenance problems, including lower productivity, erosion and corrosion. Separators are designed to efficiently remove the moisture from steam flow. The application and selection of different types are considered here.
These small items of equipment have a variety of important applications throughout steam systems and process equipment. The different types available are studied in this tutorial.
Proper condensate removal is essential to heat exchanger efficiency and long service life. An explanation of how heat exchangers operate. It introduces the subject of stall, and why and how the best trapping device is selected to maximise system efficiency.
This Block discusses the removal of condensate from heat exchange equipment supplied by saturated steam and fitted with a temperature control valve on the steam line to the heat exchanger and A steam trapping device on the condensate line from the heat exchanger.
Calculations for heat exchange applications including the design loads and the steam pressure/flowrate requirements.
Heat exchangers are often bought oversized for the required duty. This tutorial looks at the reasons why, the effects this has and related requirements, such as trap sizing for oversized exchangers.
A fully worked-through example for calculating stall and selecting a condensate removal solution for a heat exchange application.
A simple method of calculating stall is to use a stall chart. This tutorial explains the use of a chart to calculate stall for a constant secondary flowrate with a varying inlet temperature.
Not all heat exchangers are required to operate with a constant secondary flow. Typical applications might include the provision of hot water to batch processes such as tanks and vats.
Using a chart to calculate stall for a constant secondary flowrate with a varying outlet temperature.
This tutorial considers methods of overcoming condensate drainage problems, such as ensuring gravity drainage, installing an automatic pump trap device, or controlling the pressure in the steam space.
Relaying condensate back to the boiler house reduces costs. Pipe sizing and layout is discussed for drain lines, discharge lines, and pumped lines. The effects of lift and backpressure are explained; and how to reduce overall costs by utilising flash steam.
An introduction to the reasons for condensate recovery and return, including energy costs, water charges, effluent restrictions and water treatment costs. Includes sample calculations for potential savings.
Considerations surrounding the design and layout of condensate return pipework, including drain lines to steam traps, discharge lines from traps, common return lines and pumped return lines. Includes the effect of trap types used, the effect of different pressures and discharging condensate into flooded mains.
A guide to sizing condensate lines to and from steam traps, including examples and calculations using the condensate pipe sizing chart.
A basic introduction to pumping terminology, including vapour pressure and static head. Includes a description of the operation, application and comparable benefits of electrical centrifugal and mechanical condensate pumps, with sizing examples for pumps and pump discharge lines.
The benefits of recovering flash steam, how it is done and how flash steam can be applied elsewhere in the plant to maximise overall efficiency.
Recommendations for special circumstances, including lifting condensate to a higher level return line, and dealing with contaminated condensate.
Why is it necessary to desuperheat steam? What types of desuperheater exist, where are they used, and how are they installed? Basic types and more sophisticated types of desuperheater and their applications are discussed in some detail.
This tutorial introduces the common types of desuperheater in regular use, their limitations and typical applications.
Superheated steam has important advantages on certain applications, for example, when used in power stations to drive turbines. For efficient use on heating applications however, the steam must be desuperheated. This tutorial considers basic desuperheating theory and calculations.
Additional desuperheater designs such as the venturi and variable orifice types are covered in this tutorial. A comparison of all types is included at the end.
A number of important considerations need to be taken into account when installing desuperheaters. This tutorial covers issues such as water quality and pressure control. A desuperheater selection chart and a list of applications are also included.
Your closest Spirax Sarco is
This region has not yet joined our new website. You will now continue to the existing site for Spirax Sarco