30/06/2026

 

For many industrial organisations, decarbonisation has moved from a future ambition to a present-day priority.

Rising energy costs, increasing regulatory pressure and ambitious sustainability targets are driving businesses to look closely at how energy is used across their operations. Yet despite significant investment in efficiency projects, renewable technologies and carbon reduction initiatives, many organisations are still missing a critical first step.

 

The reality is simple. You cannot effectively reduce what you cannot accurately measure.

Many organisations do not have enough visibility into where energy is being consumed across their steam systems, water networks, compressed air infrastructure and manufacturing processes. Without this visibility, organisations often invest in decarbonisation projects before understanding where the greatest opportunities actually exist.

Before organisations can make informed decisions about energy efficiency, process optimisation or decarbonisation strategies, they need a clear understanding of how energy flows through their facilities. Without reliable data, even well-intentioned investments can fail to deliver the expected results.

This is why energy monitoring has become one of the most important foundations of successful industrial decarbonisation.

 

Why visibility matters in energy reduction

In many manufacturing facilities, thermal energy represents one of the largest sources of energy consumption. Steam generation, condensate recovery, hot water systems, compressed air and process heating all contribute significantly to overall energy use, yet many are monitored only at a whole-site level.

Utility bills may show total gas, electricity and water consumption, but they rarely reveal which steam users, production lines or processes are responsible for that demand, or where and when the greatest inefficiencies exist.

As a result, many organisations are forced to make decisions based on assumptions rather than evidence.

Without detailed energy data, it can be difficult to answer fundamental questions such as:

 

Which processes consume the most energy?

When does peak demand occur?

How much energy is being wasted?

Which assets are operating inefficiently?

Where should investment be prioritised?

 

These questions are central to any meaningful decarbonisation strategy.

The ability to measure energy usage in manufacturing environments provides the insight needed to identify inefficiencies, quantify opportunities and focus resources where they will deliver the greatest impact.

 

The hidden challenge of industrial energy consumption

One of the biggest obstacles to energy reduction is that many losses remain invisible.

Unlike equipment failures that stop production, energy waste often develops gradually and silently. Steam leaks, failed steam traps, compressed air losses, poorly performing heat exchangers and inefficient operating practices can continue unnoticed for months or even years.

The cumulative impact can be significant.

Many industrial sites discover that a substantial proportion of their energy consumption is linked to issues that were previously unknown because they were never measured. Many industrial sites discover that a substantial proportion of their energy consumption is either linked to issues that were previously unidentified due to gaps in energy monitoring, or known but almost impossible to quantify without the right data,

For manufacturers that rely on steam, these hidden losses can be particularly significant. Steam is often one of the largest consumers of energy on site, yet many organisations only understand how much steam they generate, not where it is used, how efficiently it is distributed or where it is being lost. Without meaningful visibility into steam consumption and system performance, inefficiencies can remain hidden while fuel costs, water consumption and carbon emissions continue to rise.

 

Data does not simply confirm what organisations already know. It often reveals opportunities they did not realise existed.

Water consumption is also closely linked to steam system performance. Every litre of make-up water introduced into a boiler must be treated, heated and pumped before it becomes useful steam. When condensate recovery is poor or excessive make-up water is required, organisations are effectively paying to heat the same water repeatedly.

Measuring both steam flow and water consumption provides valuable insight into system performance, helping identify excessive make-up rates, condensate losses and opportunities to improve efficiency while reducing operating costs, water consumption and carbon emissions.

 

Why measuring energy usage in manufacturing is the first step to decarbonisation

Decarbonisation strategies often focus on technology.

Electrification projects, heat recovery systems, renewable energy integration and alternative fuels all have an important role to play. However, implementing solutions before understanding existing performance can create unnecessary cost and complexity.

The most effective approach begins with measurement.

When organisations measure energy usage acrosstheir manufacturing processes and utilities, they establish a baseline against which future improvements can be assessed. This baseline creates a clear picture of current performance and enables businesses to set realistic targets based on actual operating conditions.

For organisations that rely on steam, this means understanding not only how much energy is consumed, but where steam, water and fuel are being used throughout the process. Metering these utilities provides the insight needed to identify inefficiencies, prioritise improvements and verify the impact of optimisation projects.

Measurement also enables organisations to:

  • Prioritise improvement opportunities

  • Quantify energy savings

  • Calculate return on investment

  • Track progress towards sustainability goals

  • Verify the effectiveness of implemented projects

  • Support reporting and compliance requirements

  • Identify and predict maintenance issues

 

 

Without this level of visibility, decarbonisation efforts become significantly more challenging.
 

Moving from reactive decisions to data driven action

Historically, many industrial energy management decisions have been reactive.

Rising utility costs trigger investigations. Equipment failures prompt maintenance activity. Sustainability targets create pressure to act quickly.

While these responses are understandable, they do not always lead to the best outcomes.

Energy monitoring allows organisations to move from reactive decision making to proactive energy management.

By continuously collecting and analysing operational data, businesses gain real time insight into system performance. Trends can be identified early,; inefficiencies can be addressed before they escalate and opportunities for improvement become easier to prioritise.

This shift from reactive to data driven decision making is increasingly becoming a competitive advantage.

Organisations that understand their energy performance are better positioned to control costs, improve efficiency and achieve sustainability objectives.

 

From energy data to operational insight

Modern monitoring and metering solutions provide visibility across the utilities and processes that have the greatest influence on operational performance. This can include monitoring:

Steam flow

Boiler performance and efficiency

Feedwater consumption

Pumped condensate return lines

Water usage

Gas consumption

Electrical demand

Compressed air systems

Heat exchangers

Steam trap operation

Process equipment and production lines

Flash steam losses

 

Together, these measurements create a comprehensive picture of how energy is consumed across a facility. Rather than viewing utilities in isolation, organisations gain a connected understanding of how steam, water, fuel and electricity interact throughout their operations.

Effective decarbonisation requires more than understanding how much electricity or gas a site consumes. Organisations increasingly need visibility into how these individual utilities influence one another and contribute to overall operational performance.

By combining steam, water, gas and electrical metering, organisations can gain valuable insight into:

  • How efficiently boilers are operating

  • Where steam demand is increasing

  • Declining steam quality / energy contents

  • Whether condensate recovery is declining

  • How effectively feedwater is being managed

  • Which production processes consume the most thermal energy

  • Where water losses are increasing operating costs

  • How energy performance changes over time

 
 

This integrated view creates a far stronger foundation for prioritising improvement projects than relying solely on utility invoices or periodic energy audits. Instead of making decisions based on assumptions, organisations can target investment where it will deliver the greatest operational, financial and environmental benefit.
For example, monitoring steam flow alongside feedwater consumption and condensate return can reveal hidden steam losses, poor condensate recovery or inefficient operating practices that may otherwise remain unnoticed.
 

Likewise, analysing water, gas and electricity consumption alongside production processes helps identify inefficiencies, establish performance baselines and verify the impact of improvement initiatives over time.

 

Importantly, industrial utility monitoring and metering is not simply about collecting more data. It is about transforming operational data into actionable insight that supports informed decision-making.

When combined with engineering expertise and analytics, measurement provides the evidence needed to make smarter operational decisions, validate energy-saving initiatives and build robust, evidence-based decarbonisation strategies.

 

Supporting sustainability goals with measurable results

Sustainability commitments are becoming increasingly important across every industry.

Customers, investors, regulators and stakeholders are demanding greater transparency around carbon reduction efforts and environmental performance.

However, demonstrating progress requires evidence.

Energy monitoring creates the data foundation needed to support sustainability reporting and carbon reduction initiatives. It enables organisations to measure improvements, verify savings and communicate results with confidence.

This is particularly important as businesses work towards Net Zero objectives and seek to demonstrate meaningful progress against environmental targets.

Reliable measurement transforms sustainability from aspiration into measurable action.

 

Turning data into decarbonisation opportunities

The journey towards decarbonisation does not begin with a new technology or a major capital project.

It begins with understanding.

Before organisations can improve efficiency, reduce emissions or optimise energy consumption, they need visibility into what is happening across their operations.

That visibility comes from measurement.

Industrial energy monitoring provides the data needed to identify waste, prioritise improvements and make informed investment decisions. It creates a clear baseline for progress and helps ensure that decarbonisation strategies are built on evidence rather than assumptions.

At Spirax Sarco, we help organisations uncover hidden opportunities within their thermal energy systems through measurement, insight and engineering expertise. By understanding how steam, water and energy are used today, businesses can make more informed decisions that improve efficiency, reduce emissions and accelerate progress towards Net Zero.

Because when organisations understand how steam, water and energy are actually being used, they can focus investment where it will deliver the greatest operational, financial and environmental impact. Decarbonisation doesn’t begin with assumptions. It begins with measurement.

 

Ready to make more informed energy decisions?

Understanding where energy is used is the first step towards reducing waste, improving efficiency and achieving your sustainability goals. Whether you're looking to establish a baseline, optimise steam system performance or accelerate your decarbonisation strategy, Spirax Sarco can help you turn operational data into meaningful action.

Speak to one of our specialists to discover how industrial utility monitoring and metering can help uncover hidden opportunities across your steam, water and energy systems.