21/10/2026

 

In manufacturing, keeping operations running smoothly is essential. But when equipment is performing as expected, maintenance can easily slip down the priority list. After all, why fix something that isn't broken?

The problem is that waiting for equipment to fail can be far more expensive than anticipated.

From unexpected production downtime and emergency repairs to wasted energy and reduced equipment lifespan, the true cost of reactive maintenance extends well beyond the initial breakdown.

For manufacturers relying on steam systems, these hidden costs can be particularly significant. Steam plays a critical role in heating, processing, sterilisation and production across industries, including food and beverage, pharmaceuticals and general manufacturing. When a component fails, the consequences can quickly affect the wider operation.

So, how can businesses move away from reactive maintenance and towards a more proactive, cost-effective approach?


What is reactive maintenance?

Reactive maintenance, sometimes referred to as breakdown maintenance, is the practice of repairing or replacing equipment only after a fault or failure has occurred.

In some circumstances, this approach may be appropriate, particularly for low-cost, non-critical components where failure has minimal operational impact.

However, when applied to essential equipment, reactive maintenance can introduce significant risks.

Consider a steam trap that has failed open. While the system may continue operating, valuable steam could be escaping unnoticed, increasing energy consumption and operating costs. Alternatively, a steam trap that has failed closed in a distribution line could cause condensate to accumulate, potentially affecting process performance and increasing the risk of waterhammer. At the point of use, a failed-closed trap can prevent effective condensate removal, leading to incorrect process temperatures, product spoilage or significant production delays.

In both scenarios, waiting until a problem becomes obvious can mean the issue has already been affecting the system for some time.

The challenge is that not every maintenance issue results in an immediate breakdown. Some failures develop gradually, quietly reducing efficiency and reliability before becoming more serious.

The hidden costs of reactive maintenance

The cost of replacing a failed component is often the most visible expense associated with reactive maintenance. However, it rarely tells the full story.

 

1. Unexpected downtime and lost production

One of the most significant consequences of reactive maintenance is unplanned downtime.

When essential equipment fails, production may need to slow down or stop entirely while engineers investigate the problem, source replacement parts and complete repairs.

For manufacturers operating to tight schedules, even relatively short interruptions can have wider consequences, including:

- Missed production targets and delayed orders
- Product spoilage or quality losses caused by incorrect process temperatures
- Increased labour and overtime costs
- Disruption to other production processes
- Reduced operational efficiency
- Additional pressure on maintenance teams

 

In facilities where steam is essential to production, an unexpected failure can affect multiple processes simultaneously.

 

Taking steps to identify and address potential issues before they escalate is therefore an important part of any strategy to reduce downtime in manufacturing.

 

2. Rising energy costs

Not all equipment failures bring production to a halt. In fact, some of the most expensive issues are those that go unnoticed.

Steam leaks, failed steam traps, poorly performing controls and damaged insulation can all contribute to unnecessary energy consumption.

For example, a steam trap that fails open can allow live steam to escape into the condensate return system. Although production may continue, the system could be consuming more energy than necessary to maintain the required performance.

Over time, these losses can accumulate, increasing fuel consumption, operating costs and associated carbon emissions. They can also increase water use and the consumption of water-treatment chemicals, adding further cost and environmental impact. For many sites, water is an important sustainability priority alongside carbon—and monitoring steam-trap performance can provide a practical route to reducing avoidable losses.

Without regular inspections and performance monitoring, businesses may be paying for energy, water and treatment chemicals that deliver little or no operational benefit.

3. Higher emergency repair costs

When equipment fails unexpectedly, maintenance becomes urgent.

Instead of scheduling repairs around planned production activities, businesses may need to arrange emergency callouts, source components at short notice or carry out work outside normal operating hours.

This can increase costs and place additional pressure on engineering teams.

A proactive maintenance strategy provides greater opportunity to plan interventions, organise resources and ensure critical spare parts are available when required.

It also helps businesses make more informed decisions about when equipment should be serviced, repaired or replaced.

4. Reduced equipment lifespan

Industrial equipment is designed to operate reliably, but its performance and lifespan depend on appropriate operating conditions and maintenance.

When minor issues are left unresolved, they can place additional stress on surrounding components.

For example, ineffective condensate removal can contribute to waterhammer, corrosion and poor heat transfer. Similarly, malfunctioning pressure controls may affect process stability and equipment performance.

By identifying these issues early, businesses can reduce the risk of secondary damage and help protect their investment in essential infrastructure.

5. Increased safety and compliance risks

Maintenance is not simply about efficiency and cost control. It also plays an important role in maintaining a safe and reliable working environment.

Steam systems operate at elevated temperatures and pressures, making appropriate inspection, maintenance and operating procedures essential.

Issues such as steam leaks, waterhammer, faulty isolation equipment and ineffective condensate management can create additional hazards if left unaddressed.

A structured maintenance programme helps identify potential concerns and supports safer system operation.

For businesses operating in highly regulated sectors, including pharmaceuticals, food manufacturing and healthcare, maintaining consistent system performance can also support wider quality and compliance requirements.

Preventative maintenance vs reactive maintenance: What's the difference?

Understanding the difference between preventative maintenance vs reactive maintenance is an important first step towards developing a more effective maintenance strategy.

While reactive maintenance focuses on responding to failures, preventative maintenance aims to reduce the likelihood of those failures occurring in the first place.

Preventative maintenance vs reactive maintenance

Reactive maintenance

Equipment is repaired after failure 

Maintenance is often unplanned 

Greater risk of unexpected downtime 

Repairs may require urgent resources

Problems may go unnoticed until failure 

Costs can be unpredictable 

 

Preventative maintenance

Equipment is inspected and serviced at planned intervals

Maintenance activities can be scheduled

Helps reduce the likelihood of unexpected failures

Labour and spare parts can be planned in advance

Developing issues can be identified earlier

Maintenance expenditure can be more predictable

 

However, preventative maintenance doesn't mean replacing every component unnecessarily or carrying out maintenance more frequently than required.

The most effective approach is based on understanding equipment condition, operational
importance and the consequences of failure.

For critical systems, this may involve combining scheduled preventative maintenance with condition monitoring and predictive maintenance techniques.

How proactive steam system maintenance can reduce downtime in manufacturing

Moving towards proactive maintenance doesn't necessarily require a complete overhaul of existing processes.

Often, the greatest improvements begin with understanding where inefficiencies and risks exist within the current system.

Here are five areas manufacturers should consider.

1. Carry out regular steam trap surveys

Steam traps play an essential role in removing condensate and non-condensable gases from steam systems while preventing unnecessary steam loss.

However, like any mechanical component, steam traps can deteriorate or fail over time—particularly if they are not correctly selected, sized, installed and maintained, or where steam quality is poor.

Regular steam trap surveys can help identify traps that are leaking, blocked or otherwise operating incorrectly.

By understanding the condition of the steam trap population, businesses can prioritise maintenance, reduce unnecessary energy losses and improve system reliability. Surveys should also assess whether process loads, building use or shift patterns have changed. If operating conditions differ from those the trap was originally selected for, its sizing or specification may need to be reviewed; otherwise, the site may experience excessive or repeated failures.

At Spirax Sarco, our steam trap surveys provide valuable insights into system performance, helping businesses identify opportunities to improve efficiency and take informed maintenance decisions.

2. Monitor steam system performance

You cannot manage what you cannot see. Just as smart meters give households clearer visibility of energy use, applying the same principle in an industrial setting can help teams understand steam-system performance and spot changes sooner.

Without sufficient visibility of steam system performance, developing issues can remain undetected until they begin affecting production.

Monitoring key parameters such as pressure, temperature, flow and energy consumption can help engineering teams understand how their systems are operating.

Where appropriate, digital monitoring solutions can provide additional insights into performance trends, helping teams identify changes that may require investigation.

This supports a more informed approach to maintenance, where decisions are based on system condition and operational data rather than waiting for equipment to fail.

3. Inspect insulation and identify steam leaks

Damaged or missing insulation and undetected steam leaks can contribute to avoidable energy losses.

Regular inspections can help identify areas where heat is escaping, particularly around pipework, valves, flanges and other steam system components.

Addressing these issues can improve thermal efficiency, reduce energy consumption and support a safer working environment.

Although individual losses may appear relatively small, their combined impact across a large steam distribution network can be significant.

4. Review condensate recovery and management

Effective condensate management is essential for maintaining steam system performance.

Condensate contains valuable thermal energy that can often be recovered and reused, reducing the demand for additional boiler feedwater and energy.

However, ineffective condensate removal can also create operational problems, including poor heat transfer, waterhammer and reduced process efficiency.

Regularly reviewing condensate return arrangements, pumping equipment and associated controls can help identify opportunities to improve reliability and system performance.

5. Plan maintenance around operational requirements

One of the biggest advantages of proactive maintenance is the ability to plan work around production schedules.

Rather than responding to unexpected failures, manufacturers can use planned shutdowns and quieter production periods to inspect equipment, complete repairs and address developing issues.

A structured maintenance plan should consider:

  • The criticality of individual components and systems

  • Equipment condition and maintenance history

  • Inspection and servicing requirements

  • Availability of critical spare parts

  • Opportunities to carry out work during planned shutdowns

  • Contingency arrangements for essential equipment

 

 

This approach helps businesses make better use of maintenance resources while reducing the likelihood of avoidable disruption.

From preventative to condition-based maintenance: The role of real-time monitoring

While preventative maintenance typically involves scheduled inspections and servicing, condition-based maintenance uses information about the actual health and performance of an asset to determine when intervention is needed.

This helps maintenance teams move beyond fixed intervals and focus attention where evidence shows deterioration, abnormal behaviour or an emerging risk. Predictive maintenance takes this further by using condition and operational data to anticipate when performance may decline or failure may occur.

For steam systems, monitoring assets and key parameters in near real time can help engineering teams recognise unusual operating conditions, identify inefficiencies and prioritise maintenance activities before production is affected.

Much like a smart meter provides visibility of energy use at home, connected monitoring can provide a clearer view of what is happening across an industrial steam system—without relying solely on periodic manual checks.

When sensors and connected monitoring are applied to critical assets, data can be collected continuously, analysed and presented as trends, alerts and actionable insights. This can help teams detect a failing steam trap or a change in process performance sooner, understand the potential impact and plan an appropriate response.

Importantly, condition-based and predictive maintenance do not eliminate the need for physical inspections or engineering expertise. Instead, they add timely evidence to support better decisions and help turn monitoring data into maintenance action.

Spirax Sarco connected solutions can support this approach by bringing asset and system information together, giving teams greater visibility of performance and helping them focus specialist support where it can deliver the most value.

The business case for proactive maintenance

For many manufacturers, the decision to invest in preventative maintenance comes down to cost.

However, focusing solely on the immediate expense of maintenance can overlook the wider financial impact of equipment failure.

A more complete assessment should consider:

The cost of doing nothing: What could an unexpected failure mean for production, energy consumption, safety and equipment condition?

The cost of intervention: What would it cost to inspect, maintain or replace equipment before failure?

The potential return: Could improvements reduce energy waste, prevent disruption or extend equipment service life?

For example, identifying and repairing failed steam traps may help reduce avoidable steam losses while improving the reliability of the wider system.

Similarly, addressing condensate recovery issues may deliver benefits beyond maintenance alone, including improved energy efficiency and reduced water consumption.

The objective is not necessarily to spend more on maintenance. It is to spend maintenance budgets more effectively, focusing resources where they can deliver the greatest operational and financial benefit.

How Spirax Sarco can support your maintenance strategy

At Spirax Sarco, we understand that reliable steam system performance is essential to keeping operations running efficiently.

Our steam engineering specialists work with businesses across the UK and Ireland to help identify opportunities to improve system performance, reduce energy losses and strengthen operational reliability.

From steam trap surveys and system assessments to technical advice, maintenance support and connected monitoring solutions, we can help you progress from planned preventative maintenance towards a more condition-based approach.

Whether you're looking to address recurring maintenance issues, improve energy efficiency or reduce the risk of unexpected downtime, understanding the condition of your existing system is a valuable place to start.

Don't wait for a breakdown to take action

Reactive maintenance may appear cost-effective in the short term, but the hidden costs of unexpected failures, wasted energy and operational disruption can quickly outweigh the initial savings.

By taking a more proactive approach, manufacturers can identify developing issues earlier, plan maintenance more effectively and improve the long-term reliability of their equipment.

When it comes to steam systems, prevention isn't just about avoiding breakdowns. It's about protecting productivity, improving efficiency and getting more value from existing assets.

Ready to take a more proactive approach to steam system maintenance?

Speak to the Spirax Sarco team today to discover how we can help you identify inefficiencies, improve reliability and keep your steam system performing at its best