Steam traps are among the most important yet overlooked components in any steam system. They operate continuously, often in demanding conditions, removing condensate while retaining valuable live steam. When they work well, they are almost invisible. When they fail, the impact is rarely noticed straight away, but the consequences can be significant.
Unlike more obvious equipment failures, a faulty steam trap does not usually trigger alarms or stop production. Instead, it can continue operating in a degraded state for long periods, quietly affecting energy use, system performance and operating costs.
Understanding how steam trap failure occurs, why it often goes undetected and what it costs in practice is key to improving both efficiency and reliability.
The role of a steam trap
A steam trap has a straightforward job. It removes condensate, air and other non-condensable gases from the system while preventing the loss of live steam.
When it is functioning correctly, it supports safe and efficient heat transfer, protects equipment and helps maintain stable process conditions. When it is not, problems can build up across the wider system.
Because steam traps are automatic and often installed in hard to access areas, they are frequently forgotten during day-to-day operations. Yet every steam system depends on them working as intended.
How steam trap failure happens
Steam traps operate in challenging conditions. High temperatures, pressure variations, corrosion, erosion and water hammer all contribute to wear over time.
As a result, steam trap failure is not unusual. It generally falls into two main categories.
Failed open
A steam trap that has failed open allows live steam to pass directly into the condensate return system.
This is often the most costly type of failure because it results in the loss of steam that has already been generated, treated and distributed.
On its own, a single failed trap may not seem significant. However, across a site with many steam traps, the cumulative effect can be substantial. Energy is wasted continuously, often without any obvious signs on the plant floor.
Failed open traps can also increase backpressure in the condensate system, which may affect overall system performance.
Failed closed
A steam trap that has failed closed prevents condensate from being discharged properly.
This leads to condensate building up within heat exchangers and process equipment. As a result, heat transfer becomes less efficient, process temperatures may become unstable and production quality can be affected.
In more severe cases, trapped condensate can contribute to water hammer, increasing the risk of equipment damage and unplanned downtime.
In the distribution pipework, a trap failed in the closed position does not directly waste steam, it can have a serious impact on productivity and operational reliability.
Why steam trap failure often goes unnoticed
One of the biggest challenges with steam trap failure is visibility.
Many traps are in areas that are not routinely monitored, such as behind equipment at height, in pipe racks or in plant rooms that receive limited inspection. Even when a trap fails, there is often no immediate external sign.
The system continues to run, production continues and the issue remains hidden.
This is particularly true for failed open traps, where live steam can be lost continuously without any obvious change in plant performance. Over time, these small losses accumulate and become a significant source of inefficiency.
The hidden cost of steam leaks
Every kilogram of steam produced represents energy, water treatment, CO2 emissions, fuel and operational cost.
When steam is lost through a failed trap, all that input energy is wasted. The boiler must generate additional steam to compensate, increasing fuel consumption and operating costs.
Individually, a single leaking trap may not appear critical. However, across a full steam system, multiple small losses can quickly add up to a meaningful financial impact.
In many cases, these losses remain undetected for long periods, quietly increasing energy bills and reducing overall system efficiency.
The impact on sustainability
Steam trap failures do not only affect cost. They also have a direct impact on environmental performance.
Every unit of wasted steam requires additional fuel at the boiler, which leads to increased carbon emissions. This makes undetected steam losses a barrier to achieving energy efficiency targets and wider sustainability commitments.
For organisations under pressure to reduce carbon output, even small improvements in steam system performance can make a measurable difference.
Identifying steam trap failure
Because steam trap issues are not always visible, proactive monitoring is essential.
Traditional approaches include manual inspections, temperature checks and ultrasonic testing. While these methods can be effective, they are often periodic and may miss developing issues between inspections.
More structured assessment provides a clearer picture of system health and helps ensure that failures are identified and addressed promptly.
Why regular steam trap surveys matter
The challenge with steam trap failure is not that it happens. All mechanical equipment will eventually wear. The real issue is detecting it early and understanding its impact.
This is where a structured steam trap survey becomes valuable.
A Spirax Sarco Steam Trap Survey provides a detailed assessment of steam trap performance across a site. Using specialist diagnostic tools and experienced engineers, each trap is evaluated to identify whether it is operating correctly or has failed.
Both failed open and failed closed traps are identified, and the associated impact on energy use is quantified. This provides a clear and practical view of where steam is being lost and what that means in real terms.
The output is a detailed report that highlights priority actions, helping maintenance teams focus resources where they will have the greatest effect.
For many sites, the findings reveal issues that have gone unnoticed for extended periods, even where maintenance routines are already in place.
By addressing these issues, organisations can reduce energy consumption, improve system reliability, lower carbon emissions and support wider operational efficiency goals.
Enhancing steam trap surveys with wireless monitoring
While periodic steam trap surveys provide valuable insight into system performance, they represent a snapshot in time. Steam traps can fail at any point between inspections, meaning losses may develop and continue unnoticed until the next survey takes place.
This is where wireless steam trap monitoring can add significant value.
Spirax Sarco's wireless steam trap monitoring solutions provide continuous visibility of steam trap performance, helping maintenance teams identify failures as they occur rather than waiting for the next inspection cycle. Sensors installed on individual traps monitor operating conditions and communicate data wirelessly to a central platform, where potential issues can be flagged automatically.
By combining regular steam trap surveys with continuous monitoring, organisations gain both a comprehensive assessment of current system health and ongoing visibility of future performance. Surveys establish a baseline and identify existing issues, while wireless monitoring helps ensure that newly developed failures are detected quickly.
This approach allows maintenance teams to move from reactive fault finding to more proactive maintenance planning. Failed open traps can be identified before energy losses become significant, while failed closed traps can be addressed before they impact process performance or equipment reliability.
For sites with a large steam trap population, limited maintenance resources or ambitious energy reduction targets, integrating wireless monitoring with a structured survey programme can provide a more complete steam trap management strategy. The result is improved reliability, greater energy efficiency and better control over steam system performance throughout the year.
Turning hidden losses into measurable gains
Steam trap failures are often silent, but their impact is not.
From energy loss and increased operating costs to reduced efficiency and environmental impact, the effects can be significant when left unchecked.
The good news is that these issues can be identified and addressed in a structured and practical way.
A Spirax Sarco Steam Trap Survey helps make the invisible visible. It provides the insight needed to understand what is happening within your steam system and highlights opportunities to improve performance across the board.
In an environment where efficiency, reliability and sustainability are under constant pressure, gaining that visibility is often the first step towards meaningful improvement.
A Spirax Sarco CSM-K clean steam generator is meeting increased demand for clean steam from a state-of-the-art sterilisation facility at Ross Hall Hospital in Glasgow.
How Spirax Sarco helped LUSH achieve sustainability and safety goals in their factory relocation project.
A major Scottish distillery is combining energy savings of more than £50,000 a year with being a better neighbour, thanks to a fl ash steam recovery system.
Plate heat exchangers from Spirax Sarco are saving energy, reducing maintenance costs and improving the comfort of patients at Leighton Hospital.
Inverted bucket traps are the most robust type of the mechanical traps.
Measures the conductivity of a liquid, degree of purity is established. The amount of dissolved solids in boiler water can be directly related to its conductivity level.