18/11/2026

 

 

Steam systems play a vital role in processes and operations across many sectors. But because steam operates at high temperatures and pressures, maintaining a safe, reliable system requires ongoing attention.

Effective steam system safety starts with understanding where risks can develop, recognising early warning signs and taking action before problems escalate. It is a preventive approach, not simply a response when something goes wrong, helping avoid equipment failure, downtime and, most importantly, risks to people.

From pressure and condensate management to ageing equipment and maintenance, there are several areas worth keeping a close eye on.


 

Managing pressure safely

Pressure is fundamental to how a steam system operates, but it also needs to be carefully controlled.

Unexpected changes in pressure can place additional stress on equipment and potentially affect the safety and reliability of the wider system. Pressure-reducing valves, safety valves and control equipment all have an important role to play in keeping operating conditions within the required limits.

Regular inspection, testing and maintenance can help ensure these components continue to perform as intended. To support safe and effective operation throughout the equipment lifecycle, Spirax Sarco can help businesses with equipment selection, commissioning and ongoing maintenance.

 

Identifying steam leaks before they become bigger problems

Steam leaks can sometimes be easy to overlook, particularly within large or complex systems, but even relatively small leaks can have an impact.

Alongside the potential safety risk of escaping steam and hot surfaces, leaks can waste valuable energy, treated water and chemicals. Over time, that can affect both operating costs and overall system efficiency.

Regular steam system assessments can help identify potential leaks and areas of deterioration before they develop into larger issues. Spirax Sarco specialists look beyond the individual component to consider how the wider system is performing. This broader view can help businesses understand where to prioritise maintenance activity.

 

Keeping steam traps working effectively

Steam traps are a relatively small part of a steam system, but when they aren’t performing correctly, the effects can be significant.

Steam trap failures can lead to two different problems: steam loss or condensate accumulation. A trap that fails open can allow live steam to escape into the condensate system, wasting energy. A trap that fails closed can cause condensate to accumulate, potentially affecting process performance and contributing to other problems within the system.

Steam trap surveys provide a practical way to understand how traps are performing across a site. Spirax Sarco’s steam trap survey services can help identify failed or underperforming traps and provide the information needed to prioritise remedial action.

 

Don’t ignore waterhammer

Banging, knocking or unusual vibration within steam pipework can be signs of waterhammer. They may indicate that condensate isn’t being removed effectively and shouldn’t simply be accepted as part of normal operation.

The resulting forces can place considerable stress on pipework, valves and other equipment. Understanding why waterhammer is occurring is therefore important, rather than simply treating the immediate symptoms.

Good system design, effective drainage and correctly selected steam traps can all help reduce the risk. Where persistent problems occur, a steam system assessment can help identify the underlying cause and determine the most appropriate corrective action.

 

Taking a proactive approach to maintenance

As steam systems age, components can deteriorate and performance can gradually change. Valves may begin to leak, steam traps can fail, insulation can become damaged and control equipment may no longer perform as effectively as it once did.

Individually, these issues may seem relatively minor. Together, however, they can have a significant impact on safety, reliability and efficiency.

Regular inspections, planned maintenance and condition assessments can help businesses build a clearer picture of their system and make more informed decisions about where to invest time and resources. These activities support effective industrial risk management in steam systems by focusing on prevention rather than simply responding to failures.

Spirax Sarco can support this through steam system surveys, maintenance services and specialist engineering expertise, helping organisations identify potential risks and opportunities for improvement across their steam and condensate systems.


Looking at the whole steam system

Steam generation, distribution, control, heat transfer and condensate recovery all interact. An issue in one part of the system can therefore have consequences elsewhere. Managing risk effectively requires looking at these connections rather than focusing on one piece of equipment in isolation.

Taking a whole-system approach can make it easier to identify potential failure points, understand the root cause of recurring problems and prioritise improvements.

With extensive expertise in steam and thermal energy systems, Spirax Sarco can work alongside engineering, maintenance and operational teams to assess existing systems and identify practical opportunities to improve safety, reliability and efficiency.

 

Reduce risk before it becomes a problem

Safe, reliable and efficient operation is the aim of a well-maintained steam system. Working towards that aim requires more than responding to equipment when it fails.

By understanding the condition of the system, addressing emerging issues and maintaining critical equipment appropriately, organisations can reduce risk while supporting dependable operation.

Are you looking to investigate a recurring problem, understand the condition of your steam traps or take a broader look at your steam and condensate system?

 

Speak to your local Spirax Sarco team to find out how a steam system assessment could help you improve safety, reliability and performance. Spirax Sarco can help you identify where attention is needed and recommend practical next steps.