16/10/2026

 

For organisations that rely on steam and thermal energy, decarbonisation has become a business priority. This includes industrial processes as well as hospitals, prisons, military bases, laboratories, universities and other large estates. Whether driven by sustainability targets, stakeholder expectations or rising energy costs, facilities, engineering and operational teams are under increasing pressure to reduce emissions while maintaining product quality, reliable services and day-to-day performance.

However, when it comes to steam and thermal energy, many organisations face the same challenge.

 

How do you reduce emissions without disrupting the process?

It is a valid concern. Steam and thermal energy are fundamental to operations in food and beverage, pharmaceuticals and manufacturing, but they are equally important in hospitals, prisons, military bases, laboratories, universities and other complex facilities. Any interruption can affect product quality and output, or the delivery of essential services such as heating, hot water, sterilisation, humidification and cleaning.

The good news is that meaningful carbon reductions do not always require major plant replacements or lengthy shutdowns. In many cases, the most effective first step is to optimise existing steam systems before considering large-scale capital investment. Just as you would not leave a hot-water tap running at home and then accept the resulting energy bill, organisations should first ensure the industrial equivalent of the “hot tap” is switched off. The same logic behind insulating homes, water pipes and windows applies at industrial scale: prevent avoidable heat loss before investing in replacement technology.


Why steam and thermal energy offer such a significant opportunity

Generating and distributing steam accounts for a substantial proportion of energy use across industrial, commercial and institutional sites. Steam remains a widely used heat-transfer medium because it can easily and reliably support both production processes and critical building services.

Over time, even well-designed steam systems naturally become less efficient. Steam traps fail, insulation deteriorates, condensate recovery reduces and control systems no longer operate at their optimum level. The demand for steam may also change, leaving infrastructure incorrectly sized for current requirements. Individually these issues may seem minor, but together they can result in significant energy waste and unnecessary carbon emissions.

Many organisations are surprised to discover that they already have untapped opportunities to improve efficiency within their existing infrastructure.

 

Optimisation before replacement

When organisations begin planning their decarbonisation strategy, there is often a focus on new technologies such as electrification, hydrogen or alternative fuels. However, this investment is unlikely to deliver value unless the organisation first understands exactly how much thermal energy is required, which processes use it and when demand occurs. Without this insight, new solutions risk being over-engineered and commercially unviable. Optimising the existing system establishes a reliable benchmark for future investment decisions.

While these technologies have an important role to play in the future, they may not always be the most practical or immediate solution.

 

Optimising existing steam systems offers several advantages.

  • It delivers measurable energy savings.
  • It reduces fuel consumption.
  • It lowers carbon emissions.
  • It often provides a faster return on investment than major capital projects.

Most importantly, many improvements can be implemented during planned maintenance periods with little or no disruption to day-to-day operations.

 

Where to start

Every site is different, but there are several areas that consistently offer opportunities for improvement.

 

Steam trap management

Steam traps are essential for removing condensate while preventing live steam loss. Steam traps that fail open can waste large amounts of energy without being immediately visible, while traps that fail closed can retain condensate and degrade the energy content and quality of the steam.

Routine surveys and continuous monitoring help identify failures quickly, improving both efficiency and system reliability.

 

Condensate recovery

Returning hot condensate to the boiler reduces the amount of energy required to heat replacement water.

Increasing condensate recovery can lower fuel consumption while also reducing water usage, chemical treatment requirements and effluent cooling costs.

This creates both environmental and operational benefits.

 

Boiler house optimisation

The boiler house often represents one of the largest energy consumers on any site that relies on steam.

Reviewing boiler sequencing, combustion efficiency, correct header configuration, blowdown management and operating pressures can reveal opportunities to reduce fuel consumption without affecting production, critical services or occupant needs.

Small adjustments can often deliver significant long-term savings.

  • Steam system insulation
  • Poor or damaged insulation allows valuable heat to escape into the surrounding environment.
  • Repairing insulation is often one of the simplest and most cost-effective ways to improve overall system efficiency while reducing unnecessary emissions.
  • Digital monitoring
  • Modern monitoring technologies provide real time visibility of steam system performance.

Rather than relying solely on periodic inspections, which are often undertaken annually, maintenance teams can use continuous monitoring to identify developing issues before they become costly failures, helping maintain both efficiency and reliability.

 

Minimising disruption through planned improvements

One of the biggest concerns surrounding decarbonisation projects is operational downtime.

Site operators understandably want to avoid anything that could interrupt production schedules, compromise critical services or affect the people who depend on the facility.

This is why many optimisation activities are best aligned with planned shutdowns or routine maintenance windows.

By integrating energy improvements into existing maintenance programmes, organisations can reduce disruption while maximising the value of scheduled downtime.

This approach also allows engineering teams to prioritise work based on operational risk and expected return.


Building a long-term decarbonisation roadmap

Reducing emissions from steam and thermal energy systems is not achieved through a single project.

  • It is an ongoing process of continuous improvement.
  • Organisations that achieve the greatest success typically follow a phased approach.
  • They begin by understanding how their current systems are performing.
  • They identify opportunities to eliminate avoidable energy losses.
  • They optimise existing assets.
  • They monitor results and use performance data to guide future investment decisions.
  • Only then do they evaluate larger infrastructure changes where they will deliver the greatest value.

This strategy reduces risk, improves confidence in investment decisions and helps ensure every step contributes towards long term sustainability goals.

 

Supporting a more sustainable future

Decarbonising steam and thermal energy does not have to mean disrupting operations or essential services.

In fact, some of the most effective carbon reduction opportunities already exist within the steam systems organisations rely on every day.

By focusing first on optimisation, organisations can reduce emissions, improve energy efficiency, lower operating costs and strengthen system reliability, all while maintaining production, services and day-to-day operations.

 

At Spirax Sarco, we work with organisations across industrial, commercial and institutional settings to identify practical opportunities for steam system optimisation and support long-term decarbonisation strategies. Whether you are taking your first steps towards Net Zero or building on existing progress, improving steam and thermal energy efficiency is one of the smartest places to start.