An eBook by Spirax Sarco UK & Ireland
Contents
1. Introduction
As the global energy landscape shifts, industries are under more pressure than ever to decarbonise but without compromising performance, uptime, or reliability.
For organisations that rely on steam, this presents a specific challenge: how do you reduce carbon emissions from a system that has, for good reason, stood the test of time?
At Spirax Sarco, we believe the answer lies not in discarding steam, but in improving how it's generated, managed, and integrated with cleaner energy sources. By combining steam with renewable technologies, and embracing hybrid solutions, businesses can unlock meaningful sustainability gains without starting from scratch.
This eBook explores how steam systems can work together with renewables to support a net-zero future.
2. Why Steam Still Matters in a Low-Carbon Future
Steam remains one of the most effective ways to deliver heat. It's consistent, controllable, and able to serve multiple loads across a plant. It’s also inherently efficient particularly when it's well-managed.
The idea that all steam must be phased out to hit carbon targets is not only unrealistic it’s also unnecessary. Steam systems can be part of the solution, not the problem.
The key lies in how we generate the steam and how that energy fits into a broader, cleaner strategy.
3. The Role of Renewables in Modern Steam Generation
There are several viable routes to integrating renewables into your steam system, and many sites are already further along than they think. Here are the most common:
a) Electrification with Renewable Power
Switching to electrically powered boilers particularly when paired with on-site or purchased renewable electricity is a straightforward way to cut Scope 1 emissions dramatically.
Electric steam boilers:
When powered by renewables (e.g., solar PV or green grid electricity), they provide a genuinely low-carbon route to steam.
b) Solar Thermal and Biomass Preheating
While full steam generation using solar or biomass is more complex, many sites are using these systems to preheat feedwater or reduce the load on existing boilers.
Solar thermal can provide warm water for condensate return systems or boiler makeup, reducing energy input. Biomass systems can be incorporated for baseload or supplementary heating.
4. Exploring Hybrid Steam Solutions
For many organisations, a fully electric or renewable solution isn’t practical on day one and that’s where hybrid systems offer real value.
What is a hybrid steam system?
A hybrid system combines traditional boiler capacity (usually natural gas or LPG) with electric or renewable-powered alternatives. The system can switch between or balance sources based on:
Benefits include:
Hybrid systems allow steam users to move forward in stages, rather than waiting for a wholesale infrastructure shift.
5. Overcoming Practical Challenges
Renewable integration is achievable, but not without its hurdles. Common challenges include:
At Spirax Sarco, we work closely with customers to develop transition plans that suit real-world sites, budgets, and timescales. Whether it’s modular installations, load sharing strategies or grant support, there’s often more room to manoeuvre than you might think.
6. Real-World Opportunities
There’s no one-size-fits-all solution, but plenty of starting points.
Here are a few examples of where renewable or hybrid solutions have worked well:
Healthcare Sector
Switching sterilisation and heating loads to electric boilers during off-peak hours, powered by green grid electricity, while retaining gas-fired units for high-demand periods.
Food & Beverage Plants
Integrating electric steam boilers for CIP (clean-in-place) processes, reducing boiler cycling and energy waste.
Pharmaceutical Manufacturing
Using biomass to preheat water and reduce the primary steam load, a measurable reduction in fuel use with minimal process impact.
Universities and Research Facilities
Implementing small electric boilers alongside legacy systems to reduce emissions from campus heat networks.
7. Where to Start
Every site is different, but the first steps are often the same:
8. Final Thoughts
There’s no need to choose between steam and sustainability.
By integrating renewable technologies and adopting hybrid systems, businesses can reduce emissions, control energy costs and take meaningful steps towards net-zero — all while maintaining the performance and reliability that steam is known for.
At Spirax Sarco, we don’t believe in a one-track solution.
We believe in practical, engineered answers to real operational challenges. And that’s what renewable steam integration is all about.
Want to know what a hybrid or renewable-ready steam system could look like for your site?
Let’s start the conversation. Our engineers are here to help you take the next step.
A Spirax Sarco CSM-K clean steam generator is meeting increased demand for clean steam from a state-of-the-art sterilisation facility at Ross Hall Hospital in Glasgow.
How Spirax Sarco helped LUSH achieve sustainability and safety goals in their factory relocation project.
A major Scottish distillery is combining energy savings of more than £50,000 a year with being a better neighbour, thanks to a fl ash steam recovery system.
Plate heat exchangers from Spirax Sarco are saving energy, reducing maintenance costs and improving the comfort of patients at Leighton Hospital.
Inverted bucket traps are the most robust type of the mechanical traps.
Measures the conductivity of a liquid, degree of purity is established. The amount of dissolved solids in boiler water can be directly related to its conductivity level.