Thermodynamic steam traps have a unique operating principle which relies on the dynamics of water and flash steam. They are simple, robust and reliable and can operate up to very high temperatures and pressures. Their construction, use and benefits are detailed here.
The thermodynamic trap is an extremely robust steam trap with a simple mode of operation. The trap operates by means of the dynamic effect of flash steam as it passes through the trap, as depicted in Figure 11.4.1. The only moving part is the disc above the flat face inside the control chamber or cap.
On start-up, incoming pressure raises the disc, and cool condensate plus air is immediately discharged from the inner ring, under the disc, and out through three peripheral outlets (only 2 shown, Figure 11.4.1, i).
Hot condensate flowing through the inlet passage into the chamber under the disc drops in pressure and releases flash steam moving at high velocity. This high velocity creates a low pressure area under the disc, drawing it towards its seat (Figure 11.4.1, ii).
At the same time, the flash steam pressure builds up inside the chamber above the disc, forcing it down against the incoming condensate until it seats on the inner and outer rings. At this point, the flash steam is trapped in the upper chamber, and the pressure above the disc equals the pressure being applied to the underside of the disc from the inner ring. However, the top of the disc is subject to a greater force than the underside, as it has a greater surface area.
Eventually the trapped pressure in the upper chamber falls as the flash steam condenses. The disc is raised by the now higher condensate pressure and the cycle repeats (Figure 11.4.1, iv).
The rate of operation depends on steam temperature and ambient conditions. Most traps will stay closed for between 20 and 40 seconds. If the trap opens too frequently, perhaps due to a cold, wet, and windy location, the rate of opening can be slowed by simply fitting an insulating cover onto the top of the trap.
Advantages of the thermodynamic steam trap
Disadvantages of the thermodynamic steam trap
The impulse trap (as shown in Figure 11.4.4) consists of a hollow piston (A) with a piston disc (B) working inside a tapered piston (C) which acts as a guide. At 'start-up' the main valve (D) rests on the seat (E) leaving a passage of flow through the clearance between piston and cylinder and hole (F) at the top of the piston. Increasing flow of air and condensate will act on the piston disc and lift the main valve off its seat to give increased flow. Some condensate will also flow through the gap between the piston and disc, through E and away to the trap outlet.
As the condensate approaches steam temperature some of it flashes to steam as it passes through the gap. Although this is bled away through hole F it does create an intermediate pressure over the piston, which effectively positions the main valve to meet the load. The trap can be adjusted by moving the position of piston (B) relative to the seat, but the trap is affected by significant backpressure. It has a substantial capacity, bearing in mind its small size. Conversely, the trap is unable to give complete shut-off and will pass steam on very light loads. The main problem however is the fine clearance between the piston and cylinder. This is readily affected by the dirt normally found in a steam system. The use of impulse traps is relatively limited so they are not considered in some subsequent sections of this Module.
Advantages of the impulse steam trap
Disadvantages of the impulse steam trap
A simple form of the labyrinth trap is shown in Figure 11.4.5. It consists of a series of baffles which can be adjusted by means of a handwheel. Hot condensate passing between the first baffle and the trap body is subject to a drop in pressure and some of it 'flashes' to steam. The space around the next baffle has to cope with an increased volume of hot condensate and prevents the escape of live steam. The baffle plates can be moved either in or out using the handwheel, which alters their position relative to the body, effectively altering the overall size of the orifice.
Advantages of the labyrinth steam trap
Disadvantages of the labyrinth steam trap
These are devices containing a hole of predetermined diameter to allow a calculated amount of condensate to flow under specific pressure conditions. In practice, condensate loads and steam pressures can vary considerably. For instance, start-up and running loads can differ considerably along with steam pressure which will change due to the actions of temperature controls. These varying conditions can result in the fixed orifice either holding back condensate in the process or passing live steam, which can affect plant performance and compromise safety.
Fixed orifices are often sized on running conditions, so that they hold back enough condensate and do not pass steam. If this is so, at start-up, they are undersized to a greater degree and the steam space stands a good chance of waterlogging.
The alternative is to size them so as not to waterlog during start-up. The hole is then effectively oversized for running conditions, and the device will pass steam. The size of hole is usually a compromise between the two conditions, such that, at some points in between, the hole is correctly sized.
Corrosion and service life of plant
Continual waterlogging significantly increases the risk of corrosion in the steam space. It is not unusual to find that after fitting fixed orifice traps, plant service life is reduced below that which may be expected with proper steam traps.
A proper steam trap should be able to achieve just sufficient capacity at all pressures and flowrates present in the application. It can then pass hot condensate without leaking steam under any condition. To achieve this, the size of the hole must vary in the trap. It must be large enough to meet the worst condition, and then have some means of reducing the effective orifice flow area when the capacity becomes too great. This exactly describes the operation of a steam trap.
Advantages of a fixed orifice trap
Disadvantages of a fixed orifice trap
Note: Fixed orifice traps are not recommended for draining condensate from any application susceptible to varying load conditions.
                            The BT6 316L stainless steel balanced pressure steam trap is specifically designed for hygienic applications including steam barriers, CIP/SIP and process vessel drainage, sterilisers and autoclaves, and culinary steam mains drainage.
                            The requirement for 316 stainless steel is gradually being extended to secondary side media such as steam and hot water.
                            The TD62LM and TD62M are maintainable high pressure thermodynamic steam traps with integral strainer and a replaceable seat to ease maintenance.