Condensate is recovered boiler feedwater that retains sensible heat and chemical treatment. Example: Returning hot condensate from a heat exchanger back to the boiler reduces fuel use compared to adding cold make‑up water.
Condensate contamination occurs when dissolved or suspended substances enter the condensate stream, altering its chemical quality. Example: Cooling water leaking through a heat exchanger tube into the condensate line.
CCD is the continuous measurement of condensate quality parameters to identify contamination events early. Example: Online conductivity monitoring installed downstream of heat exchangers.
Early detection prevents damage to boilers, piping, and downstream equipment. Example: Identifying a cooling water leak before chlorides cause boiler tube failure.
Common indicators include elevated conductivity, corrosion, scale formation, foaming, or abnormal condensate appearance. Example: A sudden rise in boiler blowdown rate caused by increased dissolved solids.
Best practice is continuous online monitoring, supported by periodic verification testing. Example: A plant relying on weekly grab samples may miss a short‑term exchanger leak.
Not without treatment or confirmation it meets feedwater quality limits. Example: Condensate contaminated with glycol is typically diverted to drain rather than returned to the boiler.
Industries with indirect heating, aggressive cleaning regimes, or complex heat exchange networks. Example: Food and beverage plants using steam‑heated pasteurisers and frequent washdowns.
Monitoring protects asset integrity and ensures stable boiler operation. Example: Preventing contaminated condensate from triggering excessive foaming in the boiler.
Contamination increases dissolved solids, requiring higher blowdown and more make‑up water. Example: A boiler burning more fuel because hot condensate is being dumped.
Energy losses increase due to higher fuel demand and reduced heat recovery. Example: Replacing 90°C condensate with 10°C make‑up water.
Heat exchanger failures, process ingress, corrosion products, and cleaning chemicals. Example: Caustic washdown fluid entering condensate during CIP operations.
It is isolated, diverted, treated, or discharged depending on contamination type. Example: Automatically dumping condensate when conductivity exceeds a set limit.
Yes, contaminants can carry over into steam and affect processes. Example: Dissolved solids leading to wet steam in a sterilisation process.
Risk can be reduced through good design, maintenance, and monitoring. Example: Regular inspection of plate heat exchangers combined with CCD.
Clean condensate usually has very low conductivity, often below 10 µS/cm. Example: Similar to demineralised water returning from a clean heat exchanger.
It indicates increased dissolved ions from contamination. Example: A sudden jump caused by cooling water containing chlorides.
Yes, online analysers provide continuous measurement and alarms. Example: Conductivity transmitters linked to a condensate dump valve.
Manual checks are periodic, end‑of‑line systems detect late, CCD detects early and continuously. Example: CCD detecting a leak immediately rather than at the boiler house.
Alarms alert operators when limits are exceeded so action can be taken. Example: An alarm triggering diversion of contaminated condensate.
Boiler and steam system standards provide guidance on water quality and monitoring. Example: Using industry boiler water guidelines to define conductivity limits.
Pure water has very low electrical conductivity. Example: Demineralised water compared to salty cooling water.
Yes, seawater causes a large and rapid conductivity increase. Example: A condenser tube leak in a coastal power plant.
Yes, dissolved salts significantly raise conductivity. Example: Brine ingress from a process heat exchanger.
Yes, most cleaning chemicals alter conductivity. Example: CIP chemicals entering condensate during plant cleaning.
Yes, milk contains dissolved solids that affect conductivity. Example: Product ingress from a dairy heat exchanger failure.
CCD insights is a digital monitoring solution that helps you detect condensate contamination earlier in your steam system.