Spirax Sarco UK
Fax: +44 (0)1242 573342
WebEnquiries@SpiraxSarco.com
http://www.SpiraxSarco.com/uk/
Spirax Sarco helps cut Northumbrian Water’s energy bill by 10%
“A reliable supply of high quality steam was a top priority on this project” says Frank Errington, works co-ordination manager for Northumbrian Water. “Without steam we couldn’t do what we do.”
Steam systems from Spirax Sarco are playing an essential role in a new green energy project that is set to cut Northumbrian Water’s annual energy bill by 10%.
The lead contractor on the project brought in Spirax Sarco to provide the boiler ancillaries and steam plant for the scheme, including a hotwell, blowdown vessel, controls, valves and sparging equipment. In addition to hardware, Spirax Sarco also provided both on- and off-site training, and is still visiting the site regularly as part of an ongoing water treatment and chemical dosing contract.
The £33 million advanced anaerobic digestion (AAD) scheme at Bran Sands, Teesport, converts sewage sludge into energy and is currently the biggest plant of its kind in the UK.
The plant uses thermal hydrolysis, which relies on injections of live steam to kill the pathogens in the sludge. Raw sludge is loaded into stainless steel vessels and the steam is injected to hold the contents at 165ºC and 6Bar. The sludge is then cooled and fed into three 7,600m3 concrete tanks, where methane-generating microbes digest it anaerobically for up to 18 days. The resulting methane is collected and used to fuel gas engines, providing a renewable source of electrical energy.
Final commissioning is now complete. The AAD plant creates enough power to make the sludge treatment process self-sufficient, with additional power providing electricity to meet half of the wider Bran Sands site’s entire energy requirements.
“Spirax Sarco has proved to be a company we can rely on and trust. Their reputation among the people on site is very good and the Spirax Sarco engineers have a good rapport with our guys, which has been very important in a groundbreaking project of this size”, says Mr. Errington.
For more information, email uk.enquiries@uk.spiraxsarco.com.
Contact us for advice from our engineers
- Help on sizing and selection
- Arrange a visit
- Answers & advice on products/applications
- Obtaining quotes & placing orders