Water Treatment Water Treatment

Spirax Sarco's water treatment expertise can help improve the performance of complete steam systems.

Spirax Sarco has solved a costly steam quality problem that persistently dogged the Centre for Life in Newcastle. The Centre's water treatment regime has been overhauled by Spirax Sarco to eliminate rapid corrosion of the steam system, which had caused the boiler feedtank to be replaced twice in four years. Frequent emergency repairs to pipework, valves, humidifiers and other steam plant components have also been eradicated.

Spirax Sarco also replaced the existing mild steel boiler feedtank, which was suffering severe corrosion, with a stainless steel version.

The Centre uses steam for humidification, washing and sterilisation. Spirax Sarco found the problems stemmed from the previous water treatment procedure. By analysing the water quality as it passed through the steam system, Spirax Sarco was able to recommend an improved mix of treatment chemicals and processes that has reduced corrosion in the boiler. A full audit of the steam distribution system, including steam traps, was also undertaken to identify and rectify blocked components.

"Before calling Spirax Sarco in to look at the problems, we had tried various solutions, but nothing had worked," explains Mr. Albert Baxter, Facilities Supervisor, Centre for Life. "We suffered regular breakdowns, blocked valves, hot water supply interruptions and even water coming through the humidification system."

Since Spirax Sarco's involvement, unplanned maintenance work on the steam system has been eliminated, according to Mr. Baxter. "We now have better quality steam, are consistently getting the right temperature hot water, and we are using less water treatment chemicals, saving further costs. We have also moved from manual to automatic boiler blowdown, which is also saving us time and money."

In addition, Spirax Sarco supplied a water quality test kit that Mr. Baxter uses daily to measure pH and Total Dissolved Solids (TDS) levels. "If any of the readings are too high or too low I can ring Spirax Sarco’s helpline and they advise me straight away what action I should take."

Spirax Sarco now has an ongoing water treatment contract with the Centre for Life and regularly visits the site to monitor and adjust the system.

Situated in the heart of Newcastle, the Centre for Life supports world-class scientific research in medicine through substantial funding and the provision of state-of-the-art facilities on site. The Centre also nurtures new bioscience companies and promotes science to the general public through an imaginative programme of exhibitions and events.

Mühendislerimize danışmak için bizimle temas kurun

  • Ürün tip ve çap seçimleri hakkında yardım
  • Ziyaret talebi
  • Ürün ve uygulamalar hakkında cevap ve tavisyeler
  • Teklif talepleri ve siparişler