Sub Saturated Water Region - Steam Table

At any pressure, water below its saturation temperature is said to be in a sub saturated state.

For example, water at a pressure of 1 atmosphere and a temperature below the saturated temperature of 100°C is sub saturated. Water at a pressure of 10 atmospheres has a saturation temperature of 180°C, and so water below this temperature is also sub saturated.

Learn more about steam in our tutorial - What is Steam?.

Set your preferences for these steam tables.

Note: - You cannot use commas (,) as decimal points. Please use periods (.)
Example: 1.02 not 1,02

Steam Saturation Curve
http://www.ukashbozdurmasitesi.com