Safety Valve Sizing

An in-depth study of the sizing process for a range of applications, including sizing equations for AD Merkblatt, DIN , TRD, ASME, API, BS6759 and others. Covers more complex issues such as two-phase flow and superheat.

Use the quick links below to take you to the main sections of this tutorial:

A safety valve must always be sized and able to vent any source of steam so that the pressure within the protected apparatus cannot exceed the maximum allowable accumulated pressure (MAAP). This not only means that the valve has to be positioned correctly, but that it is also correctly set. The safety valve must then also be sized correctly, enabling it to pass the required amount of steam at the required pressure under all possible fault conditions.

Once the type of safety valve has been established, along with its set pressure and its position in the system, it is necessary to calculate the required discharge capacity of the valve. Once this is known, the required orifice area and nominal size can be determined using the manufacturer's specifications.

In order to establish the maximum capacity required, the potential flow through all the relevant branches, upstream of the valve, need to be considered.

In applications where there is more than one possible flow path, the sizing of the safety valve becomes more complicated, as there may be a number of alternative methods of determining its size. Where more than one potential flow path exists, the following alternatives should be considered:

  • The safety valve can be sized on the maximum flow experienced in the flow path with the greatest amount of flow.
  • The safety valve can be sized to discharge the flow from the combined flow paths.

This choice is determined by the risk of two or more devices failing simultaneously. If there is the slightest chance that this may occur, the valve must be sized to allow the combined flows of the failed devices to be discharged. However, where the risk is negligible, cost advantages may dictate that the valve should only be sized on the highest fault flow. The choice of method ultimately lies with the company responsible for insuring the plant.

For example, consider the pressure vessel and automatic pump-trap (APT) system as shown in Figure 9.4.1. The unlikely situation is that both the APT and pressure reducing valve (PRV 'A') could fail simultaneously. The discharge capacity of safety valve 'A' would either be the fault load of the largest PRV, or alternatively, the combined fault load of both the APT and PRV 'A'.

This document recommends that where multiple flow paths exist, any relevant safety valve should, at all times, be sized on the possibility that relevant upstream pressure control valves may fail simultaneously.

Fig. 9.4.1  An automatic pump trap and pressure vessel system Fig. 9.4.1 An automatic pump trap and pressure vessel system

Finding the fault flow

In order to determine the fault flow through a PRV or indeed any valve or orifice, the following need to be considered:

  • The potential fault pressure - this should be taken as the set pressure of the appropriate upstream safety valve.
  • The relieving pressure of the safety valve being sized.
  • The full open capacity (Kvs) of the upstream control valve, see Equation 3.21.2.

Example 9.4.1

Consider the PRV arrangement in Figure 9.4.2.

Where:

NWP=Normal working pressure
MAAP =Maximum allowable accumulated pressure
PS=Safety valve set pressure
Po=Safety valve overpressure
PR=Safety valve relieving pressure
Fig. 9.4.2  Sizing a safety valve for a typical pressure reducing application Fig. 9.4.2 Sizing a safety valve for a typical pressure reducing application

The supply pressure of this system (Figure 9.4.2) is limited by an upstream safety valve with a set pressure of 11.6 bar g. The fault flow through the PRV can be determined using the steam mass flow equation (Equation 3.21.2):

Equation 3.21.2 Equation 3.21.2

Where:

s =Fault load (kg / h)
KV =PRV full open capacity index (KVS = 6.3)
X =Presure drop = <
P1 =Fault pressure (taken as the set pressure of the upstream safety valve) (bar a)
P2 =Relieving pressure of the apparatus safety valve (bar a)

Equation 3.21.2 is used when the pressure drop ratio is less than 0.42.

If the pressure drop ratio is 0.42 or greater, the mass flow is calculated using Equation 6.4.3.

Equation 6.4.3 Equation 6.4.3

In this example:

Since is greater than 0.42, critical pressure drop occurs across the control valve, and the fault flow is calculated as follows using the formula in Equation 6.4.3:
s = 12 Kv P1
s = 12 x 6.3 x 12.6
Therefore: s = 953 kg / h

Consquently, the safety valve would be sized to pass at least 953 kg / h when set at 4 bar g.

Once the fault load has been determined, it is usually sufficient to size the safety valve using the manufacturer's capacity charts. A typical example of a capacity chart is shown in Figure 9.4.3. By knowing the required set pressure and discharge capacity, it is possible to select a suitable nominal size. In this example, the set pressure is 4 bar g and the fault flow is 953 kg/h. A DN32/50 safety valve is required with a capacity of 1 284 kg/h.

Fig. 9.4.3  A typical safety valve capacity chart Fig. 9.4.3 A typical safety valve capacity chart

Where sizing charts are not available or do not cater for particular fluids or conditions, such as backpressure, high viscosity or two-phase flow, it may be necessary to calculate the minimum required orifice area. Methods for doing this are outlined in the appropriate governing standards, such as:

  • AD-Merkblatt A2, DIN 3320, TRD 421.
  • ASME / API RP 520.
  • BS 6759 for steam, air / gases and liquids.
  • EN ISO 4126.

The methods outlined in these standards are based on the coefficient of discharge, which is the ratio of the measured capacity to the theoretical capacity of a nozzle with an equivalent flow area.

Equation 9.4.1 Equation 9.4.1

Where:

Kd=Coefficient of discharge.

Coefficient of discharge

Coefficients of discharge are specific to any particular safety valve range and will be approved by the manufacturer. If the valve is independently approved, it is given a 'certified coefficient of discharge'.

This figure is often derated by further multiplying it by a safety factor 0.9, to give a derated coefficient of discharge. Derated coefficient of discharge is termed Kdr = Kd x 0.9

When using standard methods of calculating the required orifice area, the following points may need to be considered:

  • Critical and sub-critical flow - the flow of gas or vapour through an orifice, such as the flow area of a safety valve, increases as the downstream pressure is decreased. This holds true until the critical pressure is reached, and critical flow is achieved. At this point, any further decrease in the downstream pressure will not result in any further increase in flow. A relationship (called the critical pressure ratio) exists between the critical pressure and the actual relieving pressure, and, for gases flowing through safety valves, is shown by Equation 9.4.2.




    Equation 9.4.2







    Where:
    PB=Critical backpressure (bar a)
    P1=Actual relieving pressure (bar a)
    k=Isentropic coefficient of the gas or vapour at the relieving conditions

    For gases, with similar properties to an ideal gas, 'k' is the ratio of specific heat of constant pressure (cp) to constant volume (cv), i.e. cp : cv. 'k' is always greater than unity, and typically between 1 and 1.4 (see Table 9.4.8).

    For steam, although 'k' is an isentropic coefficient, it is not actually the ratio of cp : cv. As an approximation for saturated steam, 'k' can be taken as 1.135, and superheated steam, as 1.3. As a guide, for saturated steam, critical pressure is taken as 58% of accumulated inlet pressure in absolute terms.

  • Overpressure - Before sizing, the design overpressure of the valve must be established. It is not permitted to calculate the capacity of the valve at a lower overpressure than that at which the coefficient of discharge was established. It is however, permitted to use a higher overpressure (see Table 9.2.1, Tutorial 9.2, for typical overpressure values). For DIN type full lift (Vollhub) valves, the design lift must be achieved at 5% overpressure, but for sizing purposes, an overpressure value of 10% may be used.

    For liquid applications, the overpressure is 10% according to AD-Merkblatt A2, DIN 3320, TRD 421 and ASME, but for non-certified ASME valves, it is quite common for a figure of 25% to be used.
  • Backpressure - The sizing calculations in the AD-Merkblatt A2, DIN 3320 and TRD 421 standards account for backpressure in the outflow function,(y), which includes a backpressure correction. The ASME / API RP 520 and BS 6759 standards, however, require an additional backpressure correction factor to be determined and then incorporated in the relevant equation.
  • Two-phase flow - When sizing safety valves for boiling liquids (e.g. hot water) consideration must be given to vaporisation (flashing) during discharge. It is assumed that the medium is in liquid state when the safety valve is closed and that, when the safety valve opens, part of the liquid vaporises due to the drop in pressure through the safety valve. The resulting flow is referred to as two-phase flow.

    The required flow area has to be calculated for the liquid and vapour components of the discharged fluid. The sum of these two areas is then used to select the appropriate orifice size from the chosen valve range. (see Example 9.4.3)

    Many standards do not actually specify sizing formula for two-phase flow and recommend that the manufacturer be contacted directly for advice in these instances.
Arrow Top

Sizing equations for safety valves designed to the following standards

The following methods are used to calculate the minimum required orifice area for a safety valve, as mentioned in the most commonly used national standards.

Standard-AD-Merkblatt A2, DIN 3320, TRD 421

Use Equation 9.4.3 to calculate the minimum required orifice area for a safety valve used on steam applications:

Equation 9.4.3 Equation 9.4.3

Use Equation 9.4.4 to calculate the minimum required orifice area for a safety valve used on air and gas applications:

Equation 9.4.4 Equation 9.4.4

Use Equation 9.4.5 to calculate the minimum required orifice area for a safety valve used on liquid applications:

Equation 9.4.5 Equation 9.4.5

Where:

AO=Minimum cross sectional flow area (mm)
=Mass flow to be discharged (kg / h)
PR=Absolute relieving pressure (bar a)
ΔP=PR - PB
PB=Absolute backpressure (bar a)
T=Inlet temperature (K)
Ρ=Density (kg / m) (see Appendix A at the back of this tutorial)
M=Molar mass (kg / kmol) (see Appendix A at the back of this tutorial)
Z=Compressibility factor (see Equation 9.4.6)
αW=Outflow coefficient (specified by the manufacturer)
Ψ=Outflow function (see Figure 9.4.4)
Χ=Pressure medium coefficient (see Figure 9.4.5)

The outflow function ( Ψ ) for air and gas applications

Fig. 9.4.4  The outflow function (Ψ ) as used in AD-Merkblatt A2, DIN 3320 and TRD 421 Fig. 9.4.4 The outflow function (Ψ ) as used in AD-Merkblatt A2, DIN 3320 and TRD 421

Pressure medium coefficient (Χ) for steam applications

Fig. 9.4.5  Pressure medium coefficient (c) for steam as used in AD-Merkblatt A2, DIN 3320, TRD 421 Fig. 9.4.5 Pressure medium coefficient (c) for steam as used in AD-Merkblatt A2, DIN 3320, TRD 421

Compressibility factor (Z)

For gases, the compressibility factor, Z, also needs to be determined. This factor accounts for the deviation of the actual gas from the characteristics of an ideal gas. It is often recommended that Z = 1 is used where insufficient data is available. Z can be calculated by using the formula in Equation 9.4.6:

Equation 9.4.6 Equation 9.4.6

Where:

Z=Compressibility factor
PR=Safety valve relieving pressure (bar a)
γ=Specific volume of the gas at the actual relieving pressure and temperature (m / kg) (see Appendix A at the back of this tutorial). Note: The specific volume of a gas will change with temperature and pressure, and therefore it must be determined for the operating conditions.
M=Molar mass (kg / kmol) (see Appendix A at the back of this tutorial)
Ru=Universal gas constant (8 314 Nm / kmol K)
T=Actual relieving temperature (K)

Example 9.4.2

Determine the minimum required safety valve orifice area under the following conditions:

Consequently, the chosen safety valve would need an orifice area of at least 1 678 mm.

Two-phase flow

In order to determine the minimum orifice area for a two-phase flow system (e.g. hot water), it is first necessary to establish what proportion of the discharge will be vapour (n). This is done using the Equation 9.4.7:

Equation 9.4.7 Equation 9.4.7

Where:

n=The proportion of discharge fluid which is vapour
hf1=Enthalpy of liquid before the valve (kJ / kg)
hf2=Enthalpy of liquid after the valve (kJ / kg)
hfg2=Enthalpy of evaporation after the valve (kJ / kg)

For hot water, the enthalpy values can be obtained from steam tables.

In order to determine the proportion of flow, which is vapour, the discharge capacity is multiplied by n. The remainder of the flow will therefore be in the liquid state.

The area sizing calculation from Equations 9.4.5, 9.4.6 and 9.4.7 can then be used to calculate the required area to discharge the vapour portion and then the liquid portion. The sum of these areas is then used to establish the minimum required orifice area.

Example 9.4.3

Consider hot water under the following conditions:

Therefore, a valve must be selected with a discharge area greater than 144 mm.

Standard - ASME / API RP 520

The following formulae are used for calculating the minimum required orifice area for a safety valve according to ASME standards and the API RP 520 guidelines.

Use Equation 9.4.8 to calculate the minimum required orifice area for a safety valve used on steam applications:

Equation 9.4.8 Equation 9.4.8

Use Equation 9.4.9 to calculate the minimum required orifice area for a safety valve used on air and gas applications:

Equation 9.4.9 Equation 9.4.9

Use Equation 9.4.10 to calculate the minimum required orifice area for a safety valve used on liquid applications:

Equation 9.4.10 Equation 9.4.10

Where:

AO=Required effective discharge area (in)
=Required mass flow through the valve (lb / h)
=Required volume flow through the valve(ft / min)
1=Required volume flow through the valve (U.S. gal / min)
PR=Upstream relieving pressure (psi a)
PB=Absolute backpressure (psi a)
Cg=Nozzle gas constant (see Table 9.4.1)
T=Relieving temperature (°R °F + 460)
G=Specific gravity (ratio of molar mass of the fluid to the molar mass of air (28.96 kg / kmol)) (see Appendix A at the back of this tutorial)
Z=Compressibility factor (see Equation 9.4.6)
Kd=Effective coefficient of discharge (specified by the manufacturer)
KSH=Superheat correction factor (see Table 9.4.2)
KB=Backpressure correction factor for gas and vapour (see Figures 9.4.6 and 9.4.7)
KW=Backpressure correction factor for liquids (bellows balanced valves only) (see Figure 9.4.8)
Kµ=Viscosity factor (see Figure 9.4.9)

Nozzle gas constant for ASME / API RP 520

Table 9.4.1  Nozzle gas constant (Cg) relative to isentropic constant (k) for air and gases Table 9.4.1 Nozzle gas constant (Cg) relative to isentropic constant (k) for air and gases

The nozzle gas constant Cg is calculated using Equation 9.4.11 for air and gas applications and applied to Equation 9.4.9.

Equation 9.4.11 Equation 9.4.11

Superheat correction factors for ASME / API RP 520

Table 9.4.2  Superheat correction factors (K<SUB>SH</SUB>) as used in ASME  /  API RP 520 (Imperial units) Table 9.4.2 Superheat correction factors (KSH) as used in ASME / API RP 520 (Imperial units)

Gas and vapour constant backpressure correction factor for ASME / API 520

The backpressure correction factor (KB) is the ratio of the capacity with backpressure, C1, to the capacity when discharging to atmosphere, C2, see Equation 9.4.12.

Equation 9.4.12 Equation 9.4.12

The value of KB can be established using the curves shown in Figure 9.4.6 to Figure 9.4.8. These are applicable to set pressures of 50 psi g and above. For a given set pressure, these values are limited to a backpressure less than the critical pressure, namely, critical flow conditions. For sub-critical flow and backpressures below 50 psi g, the manufacturer should be consulted for values of KB.

  • Balanced bellows valves
Equation 9.4.13 Equation 9.4.13

Where:
PB = Backpressure (psi g)
PS = Set pressure (psi g)

Fig. 9.4.6  Constant backpressure correction factor (K<SUB>B</SUB>) for gas and vapour as used in ASME  /  API RP 520 for balanced bellows valves Fig. 9.4.6 Constant backpressure correction factor (KB) for gas and vapour as used in ASME / API RP 520 for balanced bellows valves
  • Conventional valves
Equation 9.4.14 Equation 9.4.14

Where:
PB = Backpressure (psi g)
PR = Set pressure (psi g)

Fig. 9.4.7  Constant backpressure correction factor (K<SUB>B</SUB>) for gas and vapour as used in ASME  /  API RP 520 for conventional valves Fig. 9.4.7 Constant backpressure correction factor (KB) for gas and vapour as used in ASME / API RP 520 for conventional valves

Liquid constant backpressure correction factor for ASME / API RP 520

  • Balanced bellows valves
Fig. 9.4.8  Constant backpressure correction factor (K<SUB>w</SUB>) for liquids as used in ASME / API RP 520 for balanced bellows valves Fig. 9.4.8 Constant backpressure correction factor (Kw) for liquids as used in ASME / API RP 520 for balanced bellows valves

Viscosity correction factor for ASME / API RP 520 and BS 6759

This is used to make allowances for high viscosity fluids. In order to account for this, the valve size must first be established, assuming the fluid is non-viscous. Once the size has been selected, the Reynolds number for the valve is calculated and used to establish the correction factor from Figure 9.4.9.

The valve size should then be checked to ensure that the original size chosen would accommodate the flow after the viscous correction factor has been applied. If not this process should be repeated with the next largest valve size.

Fig. 9.4.9  Viscosity correction factor (Km) as used in ASME / API RP 520 and BS 6759 Fig. 9.4.9 Viscosity correction factor (Km) as used in ASME / API RP 520 and BS 6759

The Reynolds number can be calculated using Equations 9.4.15 and 9.4.16:

Metric units - Equation 9.4.15 Metric units - Equation 9.4.15
Imperial units- Equation 9.4.16 Imperial units- Equation 9.4.16

Where:

Re=Reynolds number
=Mass flow to be discharged (kg / h)
G=Relative density / specific gravity of the liquid (dimensionless)
=Volume flow to be discharged (U.S. gal / min)
µ=Dynamic viscosity (Imperial - cP, Metric - Pa s)
AO=Discharge area (Imperial - in, Metric - mm)

Standard - BS 6759

Use Equation 9.4.17 to calculate the minimum required orifice area for a safety valve used on steam applications:

Equation 9.4.17 Equation 9.4.17

Use Equation 9.4.18 to calculate the minimum required orifice area for a safety valve used on air applications:

Equation 9.4.18 Equation 9.4.18

Use Equation 9.4.19 to calculate the minimum required orifice area for a safety valve used on gas applications:

Equation 9.4.19 Equation 9.4.19

Use Equation 9.4.20 to calculate the minimum required orifice area for a safety valve used on liquid applications:

Equation 9.4.20 Equation 9.4.20

Use Equation 9.4.21 to calculate the minimum required orifice area for a safety valve used on hot water applications:

Equation 9.4.21 Equation 9.4.21

Where:

AO=Flow area (mm)
=Mass flow to be discharged (kg / h)
=Volumetric flow to be discharged (l / s)
=Hot water heating capacity (kW)
Cg=Nozzle gas constant (see Table 9.4.3)
ΔP=PR - PB
PR=Absolute relieving pressure (bar a)
PB=Absolute backpressure (bar a)
T=Inlet temperature (K)
Ρ=Density (kg / m) (see Appendix A at the back of this tutorial)
M=Molar mass (kg / kmol) (see Appendix A at the back of this tutorial)
Z=Compressibility factor (see Equation 9.4.6)
Kdr=Derated coefficient of discharge (specified by the manufacturer)
KSH=Superheat correction factor (see Table 9.4.4)
Kµ=Viscosity correction factor (see Figure 9.4.9)

Nozzle gas constant for BS 6759

Table 9.4.3  Nozzle gas constant (C<SUB>g</SUB>) relative to isentropic coefficient (k) for gases Table 9.4.3 Nozzle gas constant (Cg) relative to isentropic coefficient (k) for gases

The nozzle gas constant Cg is calculated using Equation 9.4.22, for gases, and applied to Equation 9.4.19.

Equation 9.4.22 Equation 9.4.22

Superheat correction factor (KSH) for BS 6759

Table 9.4.4  Superheat correction factors (K<SUB>SH</SUB>) as used in BS 6759 (Metric units) Table 9.4.4 Superheat correction factors (KSH) as used in BS 6759 (Metric units)

Standard - EN ISO 4126: 2004

Use Equation 9.4.23 to calculate the minimum required orifice area for a safety valve used on dry saturated steam, superheated steam, and air and gas applications at critical flow:

Equation 9.4.23 Equation 9.4.23

Use Equation 9.4.24 to calculate the minimum required orifice area for a safety valve used on wet steam applications at critical flow; Note: wet steam must have a dryness fraction greater than 0.9:

Equation 9.4.24 Equation 9.4.24

Use Equation 9.4.25 to calculate the minimum required orifice area for a safety valve used on
air and gas applications at sub-critical flow:

Equation 9.4.25 Equation 9.4.25

Use Equation 9.4.26 to calculate the minimum required orifice area for a safety valve used on liquid applications:

Equation 9.4.26 Equation 9.4.26

Where:

Viscosity correction factor (see Figure 9.4.10)
A=Flow area (not curtain area) mm2
m=Mass flowrate (kg / h)
C=Function of the isentropic exponent (see Table 9.4.5)
Kdr=Certified derated coefficient of discharge (from manufacturer
Po=Relieving pressure (bar a)
Pb=Backpressure (bar a)
Νg=Specific volume at relieving pressure and temperature (m3/kg)
x=Dryness fraction of wet steam
Kb=Theoretical correction factor for sub-critical flow (see Table 9.4.6)
Kv=

'k' values are incorporated into the ISO 4126 standard: (Part 7). Alternatively, 'k' values can be obtained from the Spirax Sarco website steam tables.

Table 9.4.5 Value of C as a function of 'k' for steam, air and gas applications to the EN ISO 4126 standard Table 9.4.5 Value of C as a function of 'k' for steam, air and gas applications to the EN ISO 4126 standard
Table 9.4.6 Capacity correction factors for backpressure to the EN ISO 4126 standard for steam, air and gas applications -  Table 9.4.6 Capacity correction factors for backpressure to the EN ISO 4126 standard for steam, air and gas applications
Fig 9.4.10 Graph to determine k<sub>v</sub> from the Reynold's No. for liquid applications to the EN ISO 4126 standard Fig 9.4.10 Graph to determine kv from the Reynold's No. for liquid applications to the EN ISO 4126 standard

Example 9.4.4

Size the minimum flow area required for a safety valve designed to EN ISO 4126 to relieve a superheated steam system of overpressure.

Appendix A - Properties of industrial liquids

For specific gravity (G) used in ASME liquid sizing calculations, divide density by 998 (density of water).

Table 9.4.7  Properties of some common industrial liquids Table 9.4.7 Properties of some common industrial liquids

Properties of industrial gases

For specific gravity (G) used in ASME liquid sizing calculations, divide density by 998 (density of water).

Table 9.4.8  Properties of some common industrial gases Table 9.4.8 Properties of some common industrial gases
Arrow Top

What do I do now?