2
From the Mollier diagram in Figure 2.15.8, if the initial state point was saturated steam at 2 bar, the final state point was at 0.01 bar, and the expansion was isentropic, what is the approximate heat drop in one kilogram of steam?
6
From the Mollier diagram in Figure 2.15.8, if the initial state point was saturated steam at 2 bar, the final state point was at 0.01 bar, and the expansion was isenthalpic, what is the approximate heat drop in one kilogram of steam?