Fluids and Flow

Users may wish to measure the flow of steam to help with plant efficiency, energy efficiency, process control or costing purposes. This tutorial considers the characteristics of flowing fluids and the basic requirements for good steam metering practice.

Use the quick links below to take you to the main sections of this tutorial:

Arrow Top

Introduction

'When you can measure what you are speaking about and express it in numbers, you know something about it; but when you cannot measure it, when you cannot express it in numbers, your knowledge is of a meagre and unsatisfactory kind'.
William Thomson (Lord Kelvin) 1824 - 1907


Many industrial and commercial businesses have now recognised the value of:

  • Energy cost accounting
  • Energy conservation
  • Monitoring and targeting techniques

These tools enable greater energy efficiency.

Steam is not the easiest media to measure. The objective of this Block is to achieve a greater understanding of the requirements to enable the accurate and reliable measurement of steam flowrate.

Most flowmeters currently available to measure the flow of steam have been designed for measuring the flow of various liquids and gases. Very few have been developed specifically for measuring the flow of steam.

Spirax Sarco wishes to thank the EEBPP (Energy Efficiency Best Practice Programme) of ETSU for contributing to some parts of this Block.

Arrow Top

Fundamentals and basic data of Fluid and Flow

Why measure steam?

Steam flowmeters cannot be evaluated in the same way as other items of energy saving equipment or energy saving schemes. The steam flowmeter is an essential tool for good steam housekeeping. It provides the knowledge of steam usage and cost which is vital to an efficiently operated plant or building. The main benefits for using steam flowmetering include:

  • Plant efficiency.
  • Energy efficiency.
  • Process control.
  • Costing and custody.

Plant efficiency

A good steam flowmeter will indicate the flowrate of steam to a plant item over the full range of its operation, i.e. from when machinery is switched off to when plant is loaded to capacity. By analysing the relationship between steam flow and production, optimum working practices can be determined.

The flowmeter will also show the deterioration of plant over time, allowing optimum plant cleaning or replacement to be carried out.

The flowmeter may also be used to:

  • Track steam demand and changing trends.
  • Establish peak steam usage times.
  • Identify sections or items of plant that are major steam users.

This may lead to changes in production methods to ensure economical steam usage. It can also reduce problems associated with peak loads on the boiler plant.

Energy efficiency

Steam flowmeters can be used to monitor the results of energy saving schemes and to compare the efficiency of one piece of plant with another.

Process control

The output signal from a proper steam flowmetering system can be used to control the quantity of steam being supplied to a process, and indicate that it is at the correct temperature and pressure. Also, by monitoring the rate of increase of flow at start-up, a steam flowmeter can be used in conjunction with a control valve to provide a slow warm-up function.

Costing and custody

Steam flowmeters can measure steam usage (and thus steam cost) either centrally or at individual user points. Steam can be costed as a raw material at various stages of the production process thus allowing the true cost of individual product lines to be calculated.

To understand flowmetering, it might be useful to delve into some basic theory on fluid mechanics, the characteristics of the fluid to be metered, and the way in which it travels through pipework systems.

Arrow Top

Fluid characteristics

Every fluid has a unique set of characteristics, including:

  • Density.
  • Dynamic viscosity.
  • Kinematic viscosity.

Density

This has already been discussed in Block 2, Steam Engineering Principles and Heat Transfer, however, because of its importance, relevant points are repeated here.

Density (ρ) defines the mass (m) per unit volume (V) of a substance (see Equation 2.1.2).

Equation 2.1.2 Equation 2.1.2

Steam tables will usually provide the specific volume (νg) of steam at various pressures/temperatures, and is defined as the volume per unit mass:

From this it can be seen that density (ρ) is the inverse of specific volume (νg):

The density of both saturated water and saturated steam vary with temperature. This is illustrated in Figure 4.1.1.

Fig. 4.1.1 - The density (<I>ρ</I>) of saturated water (<i>ρ</i><sub>f)</sub> and saturated steam (<i>ρ</i><sub>g</sub>) at various temperatures Fig. 4.1.1
The density (ρ) of saturated water (ρf) and saturated steam (ρg) at various temperatures

Dynamic viscosity

This is the internal property that a fluid possesses which resists flow. If a fluid has a high viscosity (e.g. heavy oil) it strongly resists flow. Also, a highly viscous fluid will require more energy to push it through a pipe than a fluid with a low viscosity.

There are a number of ways of measuring viscosity, including attaching a torque wrench to a paddle and twisting it in the fluid, or measuring how quickly a fluid pours through an orifice.

A simple school laboratory experiment clearly demonstrates viscosity and the units used:

A sphere is allowed to fall through a fluid under the influence of gravity. The measurement of the distance (d) through which the sphere falls, and the time (t) taken to fall, are used to determine the velocity (u).

The following equation is then used to determine the dynamic viscosity:

Equation 4.1.1 Equation 4.1.1

Where:

μ=Absolute (or dynamic) viscosity (Pa s)
Δρ=Difference in density between the sphere and the liquid (kg/m)
g=Acceleration due to gravity (9.81 m/s)
r=Radius of sphere (m)

There are three important notes to make:

  1. The result of Equation 4.1.1 is termed the absolut or dynamic viscosity of the fluid and is measured in pascal seconds. Dynamic viscosity is also expresed as 'viscous force'.
  2. The physical elements of the equation give a resultant in kg/m, however, the constants (2 and 9) take into account both experimental data and the conversion of units to pascal seconds (Pa s).
  3. Some publications give valuess for absolute viscosity or dynamic viscosity in centipoise (cP), e.g. : 1cP = 10³ Pa s

Example 4.1.1

It takes 0.7 seconds for a 20 mm diameter steel (density 7 800 kg/m3) ball to fall 1 metre through oil at 20°C (density = 920 kg/m3).

Values for the dynamic viscosity of saturated steam and water at various temperatures are given in steam tables, and can be seen plotted in Figure 4.1.2.

Fig. 4.1.2  The dynamic viscosity of saturated water (<I>μ</I><SUB>f</SUB>) and saturated steam (<I>μ</I><SUB>g</SUB>) at various temperatures Fig. 4.1.2 The dynamic viscosity of saturated water (μf) and saturated steam (μg) at various temperatures

Kinematic viscosity

This expresses the relationship between absolute (or dynamic) viscosity and the density of the fluid (see Equation 4.1.2).

Equation 4.1.2 Equation 4.1.2

Where:
Kinematic viscosity is in centistokes
Dynamic viscosity is in Pa s
Density is in kg/m³

Example 4.1.2

In Example 4.1.1, the density of the oil is given to be 920 kg/m3 - Now determine the kinematic viscosity:

Reynolds number (Re)

The factors introduced above all have an effect on fluid flow in pipes. They are all drawn together in one dimensionless quantity to express the characteristics of flow, i.e. the Reynolds number (Re).

Equation 4.1.3 Equation 4.1.3

Where:

ρ<>= Density (kg/m)
u= Mean velocity in the pipe (m/s)
D= Internal pipe diameter (m)
μ= Dynamic viscosity (Pa s)

Analysis of the equation will show that all the units cancel, and Reynolds number (Re) is therefore dimensionless.

Evaluating the Reynolds relationship:

  • For a particular fluid, if the velocity is low, the resultant Reynolds number is low.
  • If another fluid with a similar density, but with a higher dynamic viscosity is transported through the same pipe at the same velocity, the Reynolds number is reduced.
  • For a given system where the pipe size, the dynamic viscosity (and by implication, temperature) remain constant, the Reynolds number is directly proportional to velocity.

Example 4.1.3

The fluid used in Examples 4.1.1 and 4.1.2 is pumped at 20 m/s through a 100 mm bore pipe.

Determine the Reynolds number (Re) by using Equation 4.1.3 where:
ρ = 920 kg/m
μ = 1.05 Pa s

Equation 4.1.3 Equation 4.1.3
Equation 4.1.3 Equation 4.1.3

From looking at the above Reynolds number it can be seen that the flow is in the laminar region (see Figure 4.1.7).

Flow regimes

If the effects of viscosity and pipe friction are ignored, a fluid would travel through a pipe in a uniform velocity across the diameter of the pipe. The 'velocity profile' would appear as shown in Figure 4.1.3:

Fig. 4.1.3 Velocity profile ignoring viscosity and friction Fig. 4.1.3 Velocity profile ignoring viscosity and friction

However, this is very much an ideal case and, in practice, viscosity affects the flowrate of the fluid and works together with the pipe friction to further decrease the flowrate of the fluid near the pipe wall. This is clearly illustrated in Figure 4.1.4:

Fig. 4.1.4  Velocity profile with viscosity and friction Fig. 4.1.4 Velocity profile with viscosity and friction

At low Reynolds numbers (2 300 and below) flow is termed 'laminar', that is, all motion occurs along the axis of the pipe. Under these conditions the friction of the fluid against the pipe wall means that the highest fluid velocity will occur at the centre of the pipe (see Figure 4.1.5).

Fig. 4.1.5 Parabolic flow profile Fig. 4.1.5 Parabolic flow profile

As the velocity increases, and the Reynolds number exceeds 2 300, the flow becomes increasingly turbulent with more and more eddy currents, until at Reynolds number 10 000 the flow is completely turbulent (see Figure 4.1.6).

Fig. 4.1.6  Turbulent flow profile Fig. 4.1.6 Turbulent flow profile

Saturated steam, in common with most fluids, is transported through pipes in the 'turbulent flow' region.

Fig. 4.1.7 Reynolds number Fig. 4.1.7 Reynolds number

The examples shown in Figures 4.1.3 to 4.1.7 are useful in that they provide an understanding of fluid characteristics within pipes; however, the objective of the Steam and Condensate Loop Book is to provide specific information regarding saturated steam and water (or condensate).

Whilst these are two phases of the same fluid, their characteristics are entirely different. This has been demonstrated in the above Sections regarding Absolute Viscosity (μ) and Density (ρ). The following information, therefore, is specifically relevant to saturated steam systems.

Example 4.1.4

A 100 mm pipework system transports saturated steam at 10 bar g at an average velocity of 25 m/s.

Determine the Reynolds number.

The following data is available from comprehensive steam tables:

T sat at 10 bar g= 184°C
Density (ρ)= 5.64 kg/m3
Dynamic viscosity of steam (μ) at 184°C= 15.2 x 10-6 Pa s

Where

ρ= Density= 5.64 kg/m3
u= Mean velocity in the pipe= 25 m/s
D= Internal pipe diameter= 100 mm = 0.1 m
μ= Dynamic viscosity= 15.2 x 10-6 Pa s
  • If the Reynolds number (Re) in a saturated steam system is less than 10 000 (104) the flow may be laminar or transitional.

    Under laminar flow conditions, the pressure drop is directly proportional to flowrate.
  • If the Reynolds number (Re) is greater than 10 000 (104) the flow regime is turbulent.

    Under these conditions the pressure drop is proportional to the square root of the flow
  • For accurate steam flowmetering, consistent conditions are essential, and for saturated steam systems it is usual to specify the minimum Reynolds number (Re) as 1 x 105 = 100 000.
  • At the opposite end of the scale, when the Reynolds number (Re) exceeds 1 x 106, the head losses due to friction within the pipework become significant, and this is specified as the maximum.

Example 4.1.5

Based on the information given above, determine the maximum and minimum flowrates for turbulent flow with saturated steam at 10 bar g in a 100 mm bore pipeline.

Equation 4.1.3 Equation 4.1.3

For minimum turbulent flow, Re of 1 x 105 should be considered:

Volumetric flowrate may be determined using Equation 4.1.4:

Equation 4.1.4 Equation 4.1.4

Where:

qv= Volume flow (m3/s)
A= Cross sectional area of the pipe (m2)
u= Velocity (m/s)

Mass flowrate may be determined using Equations 4.1.5 and 4.1.6:

Equation 4.1.5 - Equation 4.1.5

Where:

qm= Mass flow (kg/s)
qv= Volume flow (m3/s)
vg= S pecific volume (m3/kg)

Equation 4.1.6 is derived by combining Equations 4.1.4 and 4.1.5:

Equation 4.1.6 Equation 4.1.6

Where:

qm= Mass flow (kg/s)
A= Cross sectional area of the pipe (m2)
u= Velocity (m/s)
vg= Specific volume (m3/kg)
Arrow Top

What do I do now?