Skip Ribbon Commands
Skip to main content
×

We use cookies to give you the best experience on our website. If you continue without changing your cookie settings, we assume that you consent to our use of cookies on this device. You can change your cookie settings at any time but if you do, you may lose some functionality on our website. More information can be found in our Privacy Policy

ExpertiseSolutionsSustainability

Quick Launch

  • UK
      >
    • News
        >
      • Don’t google it – the answers to the frequently asked questions on steam are right here
News Header  

Don’t google it – the answers to the frequently asked questions on steam are right here

 

As a plant manager, specifier or operator, you probably have questions regarding ‘Steam Fundamentals’. To help you get ahead and avoid the unnecessary, and often time-consuming task of trawling Google for the answers, I’ve put together a list of the most commonly asked questions in the steam industry.

Having a solid grounding in steam fundamentals will serve you well, allowing you to achieve better safety and efficiency by planning and implementing steam and thermal energy improvements.

Read on for the answers to the frequently asked questions.

1. What is steam?

As water nears its boiling point, certain molecules build-up enough kinetic energy to momentarily escape before falling back into the liquid. Further heating of the water causes bubbles of steam to form within the water and rise-up to break through the water surface to form saturated steam. As the steam loses heat it begins to turn back into water– doing so almost immediately as it leaves the boiler. This water is known as condensate.

2. What types of steam are there?

There are three main types of steam:

• Saturated

Saturated steam is the steam that is created when water is heated to its boiling point and then vaporised with additional heat. Water in the boiler under pressure will increase the temperature of the water and the steam.

• Superheated

Superheated steam occurs when steam is at a temperature higher than its original saturation temperature.

• Flash

Flash steam is the name given to steam that is formed from hot condensate when we get a pressure drop.

3. How do boilers produce steam?

Steam is generated by heat from the combustion gases of fuel in a furnace of the boiler. This heat is then transferred to the water inside the boiler, this then evaporates the water to create steam under pressure.

4. What is a steam table?

Very briefly, saturated steam tables list the various properties of steam at differing pressures, including, saturation temperature, specific volume, and latent heat.

5. How can I use steam?

Steam is a versatile product that can be used in a number of key industries. For instance, clean steam can be used in direct injection processes in the food industry to avoid the risk of inconsistencies in product taste and taint that can result when normal culinary steam comes into contact with the end product. While in the hospitals and health industries, where clean steam forms part of the NHS’ drive to improve hospital sterilisation services, steam also generates a constant supply of hot water for hospitals and areas such as laundries and kitchens.

6. How can I monitor my steam system’s performance?

There are a range of tools that can be used to assist you in the monitoring of your steam system’s performance. The B850 Boiler House Energy Monitor offers a flexible solution for monitoring energy transfer throughout the boiler house.

Alternatively, steam system audits are available to assist you in monitoring your steam systems. These audits enable you to benchmark your entire system and its operation. Following the audit, a detailed and comprehensive report is produced to show you how well your steam system is currently performing. For those who need an extra helping-hand in monitoring their steam system and maintaining their equipment’s performance, a service contract could be ideally suited for bringing peace of mind.

7. How can I reduce the energy usage and / or costs of operating my steam system?

Energy or cost savings of up to 20 per cent can be harnessed by inviting a specialist auditor to assess your hospital or food factory’s steam system and implementing their recommendations.

Why not download our guide to ‘The Fundamentals of Steam’? Download it in your time of need by the following link, or simply print it out so you have it to hand on site: https://sxscom.uk/Fundamentals-of-steam ​​

***

STEAM BOILER FUNDAMENTALS

Providing an understanding of the wet side of the boiler and trends in plant management.