Spirax Sarco Middle East
Tel: (971) 6 5575226
Fax: (971) 6 5575246
spirax@emirates.net.ae
http://www.SpiraxSarco.com/MiddleEast/
Fax: (971) 6 5575246
spirax@emirates.net.ae
http://www.SpiraxSarco.com/MiddleEast/
Steam Flow & Heat Rate
This calculates the flowrate of saturated steam required to satisfy a heating load, such as a heat exchanger or an air heater battery operating at a specified pressure. The reciprocal calculation is also possible whereby, knowing the steam flowrate to a heat exchanger or air heater battery, the coresponding heat load can be ascertained.
Steam Flow Rate to Heat Rating - Convert the steam flowrate to any heat exchanger to the corresponding heat transfer rate.
Heat Rating to Steam Flow Rate - Convert any heat exchanger's heat rating to the corresponding steam flowrate.